Configure Modbus Access
Super users, administrators and device users can configure the settings for Modbus serial and TCP from the CLI or the web interface. The Modbus configuration options are the same in both interfaces. For more information see respective section:
The recommended settings are 19200 baud rate, 8 bit data, even parity, 1 stop bit.
Configure Modbus Serial and TCP from the CLI
-
Log in to the CLI.
-
To see the configuration options type
modbus ?.Setting Command Argument Description Help ?Shows the command help for Modbus. Modbus serial status –aenable | disableEnables or disables Modbus serial. Baud rate –br2400 | 9600 | 19200 | 38400The data transfer rate in bits per second. Parity –preven | odd | noneThe parity bit or check bit. Mode -m8e1 | 8o1 | 8n2 | 8n1Default modes for the serial configuration: - 8o1 – 8 bit data, odd parity, 1 stop bit
- 8e1 – 8 bit data, even parity, 1 stop bit
- 8n1 – 8 bit data, no parity, 1 stop bit
- 8n2 – 8 bit data, no parity, 2 stop bits
Slave address –s1 - F7The slave address or unique ID of the target device in hexadecimal. Reset settings –rDefResets all the Modbus settings to default. Modbus TCP status –tEenable | disableEnables or disables Modbus TCP. Modbus TCP port number –tP502, 5000 – 32768Sets the Modbus TCP port number to the entered value. Modbus TCP timeout -tTO1 – 64800 seconds, 0 = neverSet for how long the Modbus TCP communication can be active before timing out.
Configure Modbus Serial from the Web Interface
-
Log in to the web interface.
-
Navigate to Configuration > Network > Modbus > Serial.
-
Configure the Modbus serial settings:
-
Access: Enabled if box is checked.
-
Baud Rate: Select a baud rate [2400 | 9600 | 19200 | 38400].
-
Mode: Select a parity.
-
Target Unique ID: A unique number for the NMC, needs to be different for each NMC on a network [1 – 247].
-
-
Click Apply to save any changes.
NOTE: Reboot the NMC to apply changes. From the web interface select Control > Network > Reset/Reboot for options.
Configure Modbus TCP from the Web Interface
-
Log in to the web interface.
-
Navigate to Configuration > Network > Modbus > TCP.
-
Configure the Modbus TCP settings:
-
Access: Enabled if box is checked.
-
Port: Enter port used [502, 5000 – 32768].
-
Communication Timeout: Enter a timeout time in seconds or select never (can also enter 0 seconds for never).
-
Keep-Alive: When enabled, an acknowledge request will be sent to any open connection that has been idle for a long time (2h). This option is independent of the communication timeout setting.
-
-
Click Apply to save any changes.
NOTE: Reboot the NMC to apply changes. From the web interface select Control > Network > Reset/Reboot for options.