Configure the IP Address from the Web Interface
Log in to the web interface to change the IP address of the NMC.
To configure the TCP/IP IPv4 settings:
-
Navigate to Configuration > Network> TCP/IP > IPv4 Settings
-
Here you can:
-
Enable IPv4
-
Set a manual IP address, subnet mask and default gateway.
-
Enable BOOTP or DHCP
-
-
To enter a new manual IP address:
-
Make sure IPv4 is enabled.
-
Make sure Manual mode is selected.
-
Enter the new IP address in the field System IP.
-
Click Apply.
-
The IP address is now changed.
NOTE: Reboot the NMC to apply changes. From the web interface select Control > Network > Reset/Reboot for options.
-
To configure the TCP/IP IPv6 settings:
-
Navigate to Configuration > Network> TCP/IP > IPv6 Settings.
-
Here you can:
-
Enable IPv6
-
Enable IPv6 auto configuration
-
Set a manual IP address and default gateway.
-
Enable different DHCPv6 modes
-
-
To enter a new manual IP address:
-
Make sure IPv6 is enabled.
-
Make sure Manual Configuration is enabled and Auto Configuration is disabled.
-
Enter the new IP address in the field System IP.
-
Click Apply.
-
The IP address is now changed.
NOTE: Reboot the NMC to apply changes. From the web interface select Control > Network > Reset/Reboot for options.
-