0000649741_01_en

SNMP GET OIDs

There are several object identifiers (OID) available from the system via SNMP from the network management card (NMC). The OIDs needs to be requested with a GET from a MIB browser with correctly configured access to the NMC. The OIDs can show both analog and digital values, see respective section.

Analog Values from OIDs

The following table shows the analog values that are available as GET requests.

NOTE: Base OID Address for APC / Gutor: .1.3.6.1.4.1.318.
NOTE: If an OID is not supported it will return “No data available in this sub-tree” or “There is no such object in this MIB”.
APC / Gutor OID Address SNMP OID Name Description
1.1.1.1.1.1 upsBasicIdentModel The system model name.
1.1.1.1.1.4 upsBasicIdentModelType The detailed model information of the system used by the NMC.
1.1.1.1.2.1 upsAdvIdentFirmwareRevision The firmware revision of the system controller (MCU).
1.1.1.1.2.2 upsAdvIdentDateOfManufacture The date when the system was manufactured. In the format mm/dd/yy or yyyy.
1.1.1.1.2.3 upsAdvIdentSerialNumber A unique identifying number for the system controller (MCU) set at the factory, the number is not related to any number on the system rating plate.
1.1.1.2.1.1 upsBasicBatteryStatus Indicates the status of the battery.
  • 1 = Unknown
  • 2 = Normal
  • 3 = Low capacity
  • 4 = Fault condition
1.1.1.2.1.3 upsBasicBatteryLastReplaceDate The date when the battery were last replaced. In the format mm/dd/yy or mm/dd/yyyy.
1.1.1.2.2.1 upsAdvBatteryCapacity The calculated relative available battery capacity (of nominal battery capacity). This value will only show a useful value if the battery capacity test is started with the batteries fully charged. [%]
1.1.1.2.2.2 upsAdvBatteryTemperature The measured battery temperature by the system’s battery temperature sensor. The temperature unit depends on the NMC setting. Temperatures below zero reads as 0. [°C or °F]
1.1.1.2.2.8 upsAdvBatteryActualVoltage The battery bus voltage. [V]
1.1.1.2.2.9 upsAdvBatteryCurrent The battery current. [A]
1.1.1.2.2.27 upsAdvBatteryBreakerStatus Indicates the status of the battery breaker(s) in the system.
  • 1 = All battery breakers are open
  • 2 = At least one of the battery breakers are closed
  • 3 = Breaker status is not present
1.1.1.2.3.2 upsHighPrecBatteryTemperature The measured battery temperature by the system’s battery temperature sensor. The temperature unit depends on the NMC setting. Value is with one decimal (tenths), temperatures below zero reads as 0. [°C / °F]
1.1.1.2.3.5 upsHighPrecBatteryCurrent The measured battery current with one decimal (tenths). [A]
1.1.1.2.3.7 upsHighPrecBatteryVoltage The measured battery bus voltage with one decimal (tenths). [V]
1.1.1.3.2.4 upsAdvInputFrequency The measured frequency of the system input. [Hz]
1.1.1.3.2.12 upsAdvInputTotalActivePower The total active input power (sum of all three phases) of the system. [kW]
1.1.1.4.2.8 upsAdvOutputActivePower The total active output power (sum of all three phases) of the system. [W]
1.1.1.5.2.17 upsAdvConfigBattCabAmpHour The configured maximum ampere hours of the battery bank. The value shows the maximum battery capacity configured for the system regardless of the breaker positions. [Ah]
1.1.1.7.2.13 upsAdvTestBatteryLastDate The date of the latest performed battery discharge test. In the format YYYY-MM-DD.
1.1.1.7.2.14 upsAdvTestBatteryProcessStatus The result of the latest performed battery discharge test.
  • 1 = Successful
  • 2 = Precondition not meet
  • 3 = In progress
  • 4 = Refused
  • 5 = Cancelled
  • 6 = Pending
  • 7 = Unknown
1.1.1.7.2.15 upsAdvTestBatteryConditionStatus The result of the latest successful battery discharge test.
  • 1 = Unknown
  • 2 = Battery OK
  • 3 = Battery capacity lower
  • 4 = Battery defect
1.1.1.8.1.0 upsCommStatus The status of the communication from the SNMP agent to the system.
1.1.1.11.2.16 upsAdvStateGutorModularSpecificFaults An ASCII string containing the 64 flags representing the active specific alarms for Gutor Modular. For more information about the flags see the chapter SNMP Flags.
1.1.1.13.4.26.1.2 upsDiagSubSysNetworkComCardModelNumber The model number of the NMC.
1.1.1.13.4.26.1.3 upsDiagSubSysNetworkComCardSerialNumber The serial number of the NMC.
1.1.1.13.4.26.1.4 upsDiagSubSysNetworkComCardDateOfManufacture The manufacturing date for the NMC.
1.1.1.13.4.26.1.5 upsDiagSubSysNetworkComCardHardwareRev The hardware revision of the NMC.
1.1.1.13.4.26.1.6 upsDiagSubSysNetworkComCardFirmwareAppRev The firmware revision of the Gutor application for the NMC.
1.1.1.17.1.2.1.2 upsDCOutputStatusVoltageNominal The set nominal DC output voltage of the system with one decimal (tenths). [V]
1.1.1.17.1.2.1.3 upsDCOutputStatusCurrentRating The set output current rating of the system with one decimal (tenths). [A]
1.1.1.17.1.2.1.4 upsDCOutputStatusVoltage The measured DC output voltage of the system with one decimal (tenths). [V]
1.1.1.17.1.2.1.5 upsDCOutputStatusCurrent The measured output current of the system with one decimal (tenths). [A]
1.1.25.1.2.1.1 uioSensorStatusPortID The assigned ID of the port on the NMC where the temperature (or temperature and humidity) sensor is attached.
1.1.25.1.2.1.2 uioSensorStatusSensorID The assigned ID of the temperature (or temperature and humidity) sensor connected to the NMC.
1.1.25.1.2.1.3 uioSensorStatusSensorName The entered name of the temperature (or temperature and humidity) sensor connected to the NMC. Can be changed from the NMC interface.
1.1.25.1.2.1.4 uioSensorStatusSensorLocation The entered location of the temperature (or temperature and humidity) sensor connected to the NMC. Can be changed from the NMC interface.
1.1.25.1.2.1.5 uioSensorStatusTemperatureDegF The measured temperature by the temperature (or temperature and humidity) sensor in Fahrenheit. [°F]
1.1.25.1.2.1.6 uioSensorStatusTemperatureDegC The measured temperature by the temperature (or temperature and humidity) sensor in Celsius. [°C]
1.1.25.1.2.1.7 uioSensorStatusHumidity The measured relative humidity by the temperature and humidity sensor in percent. [%]
1.1.25.1.2.1.8 uioSensorStatusViolationStatus Indicates the reason for why an alarm is active for the sensor. Should be read as a bit map, where each bit represents if the alarm condition is active = 1 or inactive = 0.
  • Bit 1 = Maximum temperature exceeded
  • Bit 2 = High temperature exceeded
  • Bit 3 = Low temperature exceeded
  • Bit 4 = Minimum temperature exceeded
  • Bit 5 – Bit 8 = (Not used)
  • Bit 9 = Maximum humidity exceeded
  • Bit 10 = High humidity exceeded
  • Bit 11 = Low humidity exceeded
  • Bit 12 = Minimum humidity exceeded.
1.1.25.1.2.1.9 uioSensorStatusAlarmStatus The alarm status of the temperature (or temperature and humidity) sensor connected to the NMC.
  • 1 = Normal
  • 2 = Warning
  • 3 = Critical
  • 4 = N/A
1.1.25.1.2.1.10 uioSensorStatusCommStatus The status of the communication between the NMC and the connected temperature or temperature and humidity sensor.
  • 1 = Not installed
  • 2 = Communication OK
  • 3 = Communication lost
1.1.29.1.1 chargerIdentModel The model of the connected UPS or system.
1.1.29.1.3 chargerIdentSerialNumber The serial number of the connected UPS or system.
1.1.29.1.4 chargerIdentModelType The type of the connected UPS or system.
1.1.29.2.1.1.2.1 chargerInputPhaseVoltage The measured AC voltage on L1-N from the optionally connected GUMD-ADB-ACM to rectifier system 1. Requires a connected GUMD-ADB-ACM. [V]
1.1.29.2.1.1.2.2 chargerInputPhaseVoltage The measured AC voltage on L2-N from the optionally connected GUMD-ADB-ACM to rectifier system 1. Requires a connected GUMD-ADB-ACM. [V]
1.1.29.2.1.1.2.3 chargerInputPhaseVoltage The measured AC voltage on L3-N from the optionally connected GUMD-ADB-ACM to rectifier system 1. Requires a connected GUMD-ADB-ACM. [V]
1.1.29.3.1 chargerOutputStatus The current state or operation mode of the system.
  • 1 = Unknown
  • 2 = Initializing
  • 3 = Standby
  • 4 = Battery operation
  • 5 = Float charge
  • 6 = Boost charge
  • 7 = Equalizing (initial) charge
  • 8 = Direct feed
1.1.29.3.3 chargerOutputTotalCurrent The total DC output current of the rectifier modules in the system. [A]
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?