0000649741_01_en

Default User and Network Settings

Default user settings:

  • After the first log in the user is prompted and required to set a new password.

  • All users except the super user is disabled and cannot be enabled until the super user password is changed.

  • After changing the password first time the user will be directed to the network overview (path: Configuration > Network > Summary) to view the default network settings.

  • After a new user type is enabled and after the first log in the user is prompted and required to set a new password.

Default network settings:

  • HTTPS and SSH are enabled.

  • SCP is enabled but will not allow any file transfer until after the super user password has been changed from the default.

  • All other protocols are disabled.

NOTE: If a hard reset is done on the NMC the user and network settings are restored to the default settings.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?