0000649741_01_en

Network Monitoring System Overview

The network monitoring system in Gutor Modular systems provides the possibility to obtain readings, measurements, events and logs via a secure one-way communication from the controller.

The network monitoring card (NMC) is a core component of the network monitoring system. The NMC is installed inside the Gutor system and allows for multiple connection options and protocols. As an option the NMC can be combined with additional gateways for additional protocols.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?