0000649741_01_en

Change User Settings

Some user settings can be changed for all users of the same type, for example password strength requirements. Other settings are only done for a specific user, for example to change the password.

From the web interface:

  • To make changes to a specific user follow the path: Configuration > Security > Local Users > Management and then click on the name of the specific user.

  • To make changes to a type of users follow the path: Configuration > Security > Local Users > Default Settings

From the CLI type user ? to view the available options. For example, to set the password of a user, type user –n <user name> –pw <new password>.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?