0000649741_01_en

Network Management Card Overview

The network management card (NMC) makes it possible to access logs, status information and events from Gutor systems.

The information can be accessed with:

  • Graphical user interface (GUI) also called the web interface, with remote access from a web browser

  • Command line interface (CLI), with both local and remote access options

  • Simple network management protocol (SNMP)

  • Modbus

NOTE: A proxy server cannot be used to access the NMC.

Benefits of an NMC in a Gutor System

With an NMC you can:

  • Monitor and manage your Gutor systems remotely over your own enterprise network.

  • Identify trends and take preventive actions.

  • Manage and maintain battery systems. See detailed battery information that can be used to plan preventive maintenance.

  • Monitor external triggers that can initiate actions on other connected devices (for example air conditioning).

  • Be ready to support the next generation of IP network.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?