0000649741_01_en

SNMPv1 Access

SNMPv1 uses access communities to define what IP addresses on the network have access to the SNMP communication from the NMC.

SNMPv1 Access Communities

To use SNMPv1 an access community is used. Each access community has a community name, a IP name or a host name and an access type. It is possible to defined up to four different access communities.

  • The community name: Used for access by a network management station (NMS). The maximum length of a community name is 15 ASCII characters.

  • The NMS IP/host name: The IPv4 or IPv6 address, IP address mask, or host name that controls access by NMSs. A host name or a specific IP address (for example, 149.225.12.1) allows access only by the NMS at that location. IP addresses that contain 255 restrict access as follows:

    • 149.225.12.255: Access by NMS on the 149.225.12 segment.

    • 149.225.255.255: Access by NMS on the 149.225 segment.

    • 149.255.255.255: Access by NMS on the 149 segment.

    • 0.0.0.0 (the default setting) which can also be expressed as 255.255.255.255: Access by NMS on any segment.

  • The access type: There are four different access types:

    • Read: GETS only, at any time

    • Write: GETS at any time, and SETS when no user is logged onto the UI or command line interface.

    • Write+: GETS and SETS at any time.

    • Disable: No GETS or SETS at any time.

Configure SNMPv1 from the CLI

  1. Log in to the CLI.

  2. To see the configuration options type snmpV1 ?.

    NOTE: In the table [n] is the access community number 1, 2, 3 or 4.

    Setting Command Argument Description
    Help ?   Shows the command help.
    SNMPv1 access –s enable | disable Enables or disables SNMP version 1.
    Community name –c[n] <Community Name> Specify a community name.
    Community access type –a[n] read | write | writeplus | disable Set the access type of a community.
    Community IPv4/IPv6 address or host name –n[n] <IP address> | <Host Name> Specify the IPv4/IPv6 address or the host name of community.

Configure SNMPv1 from the Web Interface

  1. Log in to the web interface.

  2. Navigate to Configuration > Network > SNMPv1 > Access Control.

  3. Click on a community name to configure Community Name, NMS IP/Host Name and Access Type.

  4. Click Apply to save any changes.

    NOTE: Reboot the NMC to apply changes. From the web interface select Control > Network > Reset/Reboot for options.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?