0000649741_01_en

Reset Password

To reset the password all the NMC must be reset to its default settings. This will remove all the configurations on the NMC, including the passwords.

To reset the NMC:

  1. Hold down the Reset button for 20-25 seconds, as long as the status LED is green.

  2. As soon as the status LED changes to orange release the Reset button.

  3. Let the NMC reboot and start up again.

  4. The IP address, network settings, user settings and any other settings will need to be configured again.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?