0000649741_01_en

Overview of the Web Interface

The default Home page is shown when logged in to the web interface. This is an example of the default Home page:

The default home page has two main sections, Device and Recent Device Events. The Main Menu and the Quick Status Menu are always displayed on all pages and subpages.

  • (A) Device: System status overview.
  • (B) Recent Device Events: Lists the latest events.
  • (C) Quick Status Menu: Quick overview and some common menu options.
  • (D) Main Menu: The main navigation menu.

Home Page: Device

The Device section shows the system or unit type, name and location. The section provides information on any alarms that are present in the system.

Home Page: Recent Device Events

The Recent Device Events contains a list of the latest events with the most recent at the top. Click More Events > to view the full list of events.

Each event contains a date, time and event description. The color of the event also gives a quick overview of the event type.

It is possible to enable/disable color coded events. To do that navigate to Configuration > Security > Local Users > Default Settings, then under User Preferences there is a check box for Event Log Color Coding.

Event Text Color Event Severity Severity Description
Red/Orange Critical A critical alarm exists and requires immediate action.
Yellow Warning An alarm exists and requires attention. If not addressed, it could damage data or equipment.
Green Alarm Cleared The alarm has been resolved and cleared.
Black Normal No alarms are present. The NMC and all connected devices are operating normally.
Blue Informational An event to provide information. The NMC and all connected devices are operating normally.

Quick Status Menu

The Quick Status Menu in the top right corner contains an overview of the alarms and some setting options:

  • System status: Shows if the system operates as intended or the number of present alarms and warnings.

  • User name: Click to configure the user preferences.

  • Language: The current displayed language

  • Log Off: Logs out the user from the web interface.

  • Help: Opens a new window that provides help for the current page in the web interface. In the help window it is possible to navigate and view help for each page.

  • Pin: Click to set the current page as the new home page, the icon will change to a pushed in pin (circle). Click again to reset to the default home page.

Main Menu

The Main Menu is used to navigate between the pages. The pages and navigation options are:

  • Home: Returns the user to the Home page.

  • Status: Sub menus for status and measurements from the system, modules, breakers, sensors and network.

  • Control: See current login sessions and reset network settings.

  • Configuration: Configure system information and sensor, security, network and notification settings. Can also configure general settings for the interface and Syslog settings.

  • Test: Test the LEDs on the NMC.

  • Logs: Look at, download or change size of the event logs and the data logs. View the firewall policy log.

    NOTE: By default the size of the event log and data log is set to 400 entries (maximum 1500 entries).
  • About: View the information about the system, network settings and firmware. Contains information for troubleshooting.

For a detailed description of all pages and feature, please see the Help page available from the Quick status Menu.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?