0000649741_01_en

SNMP Access to the Network Management Card

SNMP is an internet standard protocol for IP networks. The NMC supports SNMPv3, SNMPv2c over SNMPv1 and SNMPv1.

With SNMP a Network Management System (NMS) can access the NMC by configuring a user profile (SNMPv3) or a community (SNMPv1). To view the traps a trap receiver also needs to be configured for the NMS.

Super users, administrators and network only users can configure the settings for SNMPv3 and SNMPv1 from the CLI or the web interface.

NOTE: Gutor system ignores any SET commands, only GET commands and traps can be used.
NOTE: Both SNMPv3 and SNMPv1 are disabled by default. There are no default settings available. The settings need to be defined before it is possible to enable the protocols.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?