0000649741_01_en

How to Change the IP Address from the CLI with Local Connection

When connected and logged in to the CLI the IP address of the NMC can be changed.

To set a new IPv4 TCP/IP address:

  1. Type tcpip –i xxx.xxx.xxx.xxx where xxx.xxx.xxx.xxx is the new IPv4 address.

  2. Press Enter.

  3. The IP address is now changed.

To set a new IPv6 TCP/IP address:

  1. Type tcpip6 –i xxxx:xxxx:xxxx:xxxx:xxxx:xxxx:xxxx:xxxx where xxxx:xxxx:xxxx:xxxx:xxxx:xxxx:xxxx:xxxx is the new IPv6 address.

  2. Press Enter.

  3. The IP address is now changed.

    NOTE: Reboot the NMC to apply changed. From the CLI type reboot and press Enter.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?