0000649741_01_en

Command Line Interface

The command line interface (CLI) is one of the interfaces used to connect to the NMC.

The CLI can be accessed locally from the Micro-USB Console port on the NMC. It is also possible to connect remotely using SSH or Telnet.

From the CLI a user can access the same information that is available from the web interface, but the settings options are slightly different.

NOTE: The CLI is only available in English.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?