SNMP Trap OIDs
Any active traps can be view from a management information base (MIB) browser with correctly configured trap receiver connected to the NMC. Make sure that the MIB is used so that the traps can be identified.
The following table shows the different traps that can be sent out from the NMC when triggered. The NMC will only send out the traps that are currently triggered in the system.
| SNMP Trap | Description |
|---|---|
| communicationLost (1) | Communication to the system has been lost. Steps to reestablish communication are in progress. |
| upsCriticalCondition (734) | A critical condition that requires immediate action is detected. The first variable is the critical condition text message. The second variable is the critical condition number. |
| upsWarningCondition (736) | A warning condition that requires action is detected. The first variable is the warning condition. |
| upsInformationalCondition (738) | An informational condition is detected. The first variable is the informational condition. |