DOCA0147EN-17

Firmware Version 003.005.003

New Features

The following features are added:

  • The MasterPacT MTZ circuit breakers are now discoverable devices.

  • Integration of secure email.

Bugs Fixed

The following bugs are fixed:

  • IFE interface time and date were not well synchronized with the SNTP server.

  • Refresh of data on IFE interface stopped after a few hours of use.

  • IP filtering was disabled after a firmware update of IFE interface.

  • IFE interface and IO module ULP communication did not share the correct cradle status when powered up with a device in disconnected position.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?