DOCA0147EN-17

Firmware Version 005.003.000

New Features

  • Enabled ULP communication for the MasterPacT MTZ circuit breakers with MicroLogic Active control unit and BCIM module.

  • Added IO MODULES page under MONITORING & CONTROL tab, where you can view input/output configuration of IO modules connected to the IFE or EIFE interface.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?