Installation Procedure
DANGER |
|---|
|
HAZARD OF ELECTRIC
SHOCK, EXPLOSION, OR ARC FLASH
Failure to follow these instructions will result in death or serious injury.
|
| NOTICE |
|---|
|
EQUIPMENT DAMAGE
Keep this product stabilized in the panel cut
while you are installing or removing the screw fasteners.
Failure to follow these instructions can result in equipment damage.
|
| NOTICE |
|---|
|
BROKEN
ENCLOSURE
Do not exert more torque than the amount specified.
Failure to follow these instructions can result in equipment damage.
|
- Check that the gasket is seated securely into the bezel’s
groove, which runs around the perimeter of the display panel frame.NOTE: Always use the installation gasket, since it absorbs vibration in addition to repelling water. For the procedure on replacing the installation gasket, refer to Replacing the Installation Gasket.
- Based on the Panel Cut Dimensions, open a mount-hole on the panel and attach this product to the panel from the front side.
- Confirm that the anti-drop lock on the top of this product is attached to the panel.
- Insert the installation fasteners into the bracket openings at the top, bottom, left and right, and use a screwdriver to tighten the screws little by little, alternating between diagonally-positioned screws.
DANGER