DOCA0054EN-10

IO Module Registers

Introduction

This section describes the IO module registers.

Registers 13824 to 15719 are held by the IO 1.

Registers 16824 to 18719 are held by the IO 2:

  • The registers of the parameters of IO 2 are equal to the registers of the parameters of IO 1 plus 3000.

    Example:

    • Register 14599 holds the digital input status register of the IO 1.

    • Register 17599 holds the digital input status register of the IO 2.

  • The order of the registers is the same as that of the IO 1.

  • The characteristics (access type, size, range, and unit) are the same as those of the registers of IO 1.

  • Registers 15360 to 16109 containing the predefined application are specific to the IO 1 because they hold the predefined applications.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?