DOCA0054EN-10

Circuit Breaker Manager Event Log

General Description

The system stores the events that concern circuit breaker control (for example opening or closing of the contacts) in the file number 30.

This file is made up of 100 records and each record is made up of five registers.

This file is reset in case of 24 Vdc power loss on the BCM ULP module or change of the communication parameter 4W/2W + ULP.

File Header

The following table describes the file header content:

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x02CD

718

R

INT16U

A/E/P/H

File status:

0x0000 = file disabled

0xFFFF = file enabled (factory setting)

0x02CE

719

R

INT16U

A/E/P/H

Type of file = 30

0x02CF

720

R

INT16U

A/E/P/H

File allocation = 0xFFFF

0x02D0

721

R

1

INT16U

A/E/P/H

Size of a record = 5 registers

0x02D1

722

R

INT16U

A/E/P/H

File filling mode:

0 = circular

File Status

The following table describes the file status content:

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x02DD

734

R

1

INT16U

100

A/E/P/H

Size of a file = 100 records

0x02DE

735

R

1

INT16U

5

A/E/P/H

Size of a record = 5 registers

0x02E0

737

R

1

INT16U

0–100

A/E/P/H

Number of records in the file

0x02E1

738

R

1

INT16U

0–8000

A/E/P/H

Sequence number of first record in the file (the oldest)

0x02E2

739

R

1

INT16U

0–8000

A/E/P/H

Sequence number of last record in the file (the most recent)

0x02E3– 0x02E5

740–742

R

DATE

P/H

Date of the last file reset

Factory setting = 0x8000 0x8000 0x8000

Event Record

The following table shows the format of 1 record in the event log of the circuit breaker:

Registers

Type

Description

1–4

XDATE

Event date

5

INT16U

Event number (see table below)

Events

The following table shows the events in the event log of the circuit breaker:

Event Number

Description

1

RESET or system energized

2

Configuration data stored in the cradle manager

3

Spring charged

4

Circuit breaker opened (O)

5

Circuit breaker closed (F)

6

Circuit breaker tripped (SD)

7

Circuit breaker fault tripped (SDE)

8–9

Reserved

10

Closing command input remotely (AUTO) (XF)

11

Opening command input remotely (AUTO) (MX)

12

Modification of Modbus configuration (address, Baud rate, and parity)

13

Event log reset

14

Clock update input locally accepted

15

Clock update input locally rejected

(synchronization by the supervisor)

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?