Schematics with MasterPact NT/NW and ComPact NS Circuit Breakers
Description
Depending on the type of circuit breaker used, connect the IFE interface to the circuit breaker using one of the following configurations:
-
Connection of the IFE interface to a fixed manually-operated ComPact NS circuit breaker with a BCM ULP module.
-
Connection of the IFE interface to a fixed electrically-operated MasterPact NT/NW or ComPact NS 630b-1600 circuit breaker with a BCM ULP module.
-
Connection of the IFE interface to a drawout MasterPact NT/NW or ComPact NS 630b-1600 circuit breaker with a BCM ULP module and its respective IO module.
For more information, refer to the ULP System User Guide.
ULP Connection
| NOTICE |
|---|
|
HAZARD OF EQUIPMENT DAMAGE
Failure to follow these instructions can result in equipment damage.
|
All connection configurations require the BCM ULP cord.
Connection of the IFE Interface to a Fixed Manually-Operated ComPact NS Circuit Breaker
Connection of the IFE Interface to a Fixed Electrically-Operated MasterPact NT/NW or ComPact NS 630b-1600 Circuit Breaker
Connection of the IFE Interface to a Drawout MasterPact NT/NW or ComPact NS 630b-1600 Circuit Breaker

A IFE Ethernet interface for one circuit breaker
B ULP line termination
C RJ45 ULP cord
D Circuit breaker BCM ULP cord
E Circuit breaker disconnected position contact (CD)
F Circuit breaker cradle
G BCM ULP circuit breaker communication module
H Drawout circuit breaker
I Drawout terminal block
J Circuit breaker connected position contact (CE)
K Circuit breaker test position contact (CT)
L IO input/output application module for one circuit breaker