DOCA0054EN-10

Time-Stamped Information

General Description

The time-stamped information enables to know all the dates relative to important information (date of last trip, date of last actuation of MX, XF release).

Date of Last Event

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x029E–0x02A0

671–673

R

DATE

A/E/P/H

Date of last actuation of MX auxiliary

0x02A2–0x02A4

675–677

R

DATE

A/E/P/H

Date of last actuation of XF auxiliary

0x02A6–0x02A9

679–682

R

XDATE

A/E/P/H

Current date of BCM ULP module

0x02AB–0x02AD

684–686

R

DATE

A/E/P/H

Date of last circuit breaker opening

0x02AE–0x02B0

687–689

R

DATE

A/E/P/H

Date of last circuit breaker closing

0x02B1–0x02B3

690–692

R

DATE

A/E/P/H

Date of last trip without an electrical fault

0x02B4–0x02B6

693–695

R

DATE

A/E/P/H

Date of last trip with an electrical fault

0x02B7–0x02B9

696–698

R

DATE

A/E/P/H

Date of last “PF ready to close” status

0x02BA–0x02BC

699–701

R

DATE

A/E/P/H

Date of last “End of opening order” event.

This event occurs when:

  • there is no action on the opening pushbutton on the front of the device

  • the fault-trip reset pushbutton is in (the device is reset)

  • the MN undervoltage release is powered (if present)

0x02BD–0x02BF

702–704

R

DATE

A/E/P/H

Date of last “CH spring charged” status

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?