Configuration of the M2C/M6C Programmable Contacts
General Description
The M2C and M6C programmable contacts may be used to signal pick-up value overruns or status changes:
-
M2C has two contacts, 1 and 2
-
M6C has six contacts, 1 to 6
The M2C/M6C programmable contacts can be configured:
-
locally via the HMI of the MicroLogic P/H trip unit
-
remotely via the communication interface
The remote configuration of each contact can be allowed or forbidden by the local configuration via the HMI of the MicroLogic P/H trip unit with a firmware version > 2009 AJ.
Remote Configuration Status
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
---|---|---|---|---|---|---|---|---|
0x2647 |
9800 |
R |
– |
– |
INT16U |
0–1 |
P/H |
Remote configuration status: 0 = indicates that remote configuration of the contact is not authorized (factory setting). 1 = indicates that remote configuration of the contact is authorized. Remote configuration status can be modified only locally via the HMI of MicroLogic P/H trip unit. |
M2C/M6C Programmable Contact Registers
The settings of the M2C/M6C programmable contacts are in the contact registers:
Contact Number |
Contact Addresses |
Contact Registers |
---|---|---|
1 |
0x2648–0x264E |
9801–9807 |
2 |
0x264F–0x2655 |
9808–9814 |
3 |
0x2656–0x265C |
9815–9821 |
4 |
0x265D–0x2663 |
9822–9828 |
5 |
0x2664–0x266A |
9829–9835 |
6 |
0x266B–0x2671 |
9836–9842 |
M2C/M6C Programmable Contact 1 Description
The order and the description of the M2C/M6C programmable contacts are the same as that of contact 1:
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
---|---|---|---|---|---|---|---|---|
0x2648 |
9801 |
RW |
– |
– |
INT16U |
0–4 |
– |
Output mode |
E/P/H |
0 = normal (non-latching) mode (factory setting) Contact closed each time for as long as the assigned alarm remains active. |
|||||||
P/H |
1 = latching mode Contact closed for each assigned alarm and remains activated until the alarm is reset by the user (through the command interface or by a reset on the trip unit). |
|||||||
P/H |
2 = time delay mode Contact closed for a set time for each assigned alarm. It is opened at the end of the time delay whether the alarm is still active or not. The alarm must change status at least once to open the contact again. |
|||||||
E/P/H |
3 = forced to 1 The contact remains closed and is not controlled by the alarm status. |
|||||||
E/P/H |
4 = forced to 0 The contact remains open and is not controlled by the alarm status. |
|||||||
0x2649 |
9802 |
RW |
10 |
s |
INT16U |
10– 3600 |
P/H |
Contact activation time delay for time-delay mode Factory setting: 3600 (360 s) |
0x264A–0x264D |
9803– 9806 |
RW |
– |
– |
OCTET STRING |
0x00– 0x7F |
P/H |
Contact name in ASCII (A–Z and 0–9) using 4 registers Update via the trip unit not possible Factory setting: |
0x264E |
9807 |
RW |
– |
– |
INT16U |
1000– 1031 |
E/P/H |
Owner alarm number for the contact 1. Factory setting = 0x8000 (no owner) |
Type of Programmable Contacts
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
---|---|---|---|---|---|---|---|---|
0x2672 |
9843 |
R |
– |
– |
INT16U |
0–6 |
E/P/H |
0 = none |
E/P/H |
2 = M2C |
|||||||
P/H |
6 = M6C |
Event Assignment to M2C/M6C Programmable Contacts
The M2C/M6C programmable contacts can be associated to a basic or advanced protection parameter event.
Depending on the protection parameter, a specific register can contain the programmable contact number which opens or closes at the end of the protection time delay (register 8763 as example).