DOCA0054EN-10

Digital Inputs

Digital Input Register Mapping

Each digital input description is made up of 80 registers.The order and the description of the digital inputs 2, 3, 4, 5, and 6 are the same as those of digital input 1.

IO Module

Digital Input Number

Digital Input Addresses

Digital Input Registers

IO 1

I1

0x3669–0x36B8

13930–14009

I2

0x36B9–0x3708

14010–14089

I3

0x3709–0x3758

14090–14169

I4

0x3759–0x37A8

14170–14249

I5

0x37A9–0x37F8

14250–14329

I6

0x37F9–0x3848

14330–14409

IO 2

I1

0x4221–0x4270

16930–17009

I2

0x4271–0x42C0

17010–17089

I3

0x42C1–0x4310

17090–17169

I4

0x4311–0x4360

17170–17249

I5

0x4361–0x43B0

17250–17329

I6

0x43B1–0x4400

17330–17409

Digital Input 1 Registers of IO 1

The order and the description of the digital input 1 registers of IO 2 are the same as those of IO 1:

Address

Register

RW

Unit

Type

Range

Bit

Description

0x3669

13930

R

INT16U

Quality of each bit of register 13931:

  • 0 = Invalid

  • 1 = Valid

0x366A

13931

R

INT16U

0

Digital input status:

  • 0 = Off

  • 1 = On

1

Digital input forced status:

  • 0 = Unforced

  • 1 = Forced

2–15

Reserved

0x366B–0x366E

13932–13935

R

DATETIME

Timestamp for the last input transition:

  • Last rising edge if input is configured as NO (normally open contact)

  • Last falling edge if input is configured as NC (normally closed contact)

Valid if input signal type is a normal digital input (not valid for pulse digital input).

0x366F–0x3670

13936–13937

Reserved

0x3671–0x3672

13938–13939

R

INT32U

0–4294967294

Input counter value

This counter increments for each rising edge of the input.

Valid if input signal type is normal digital input.

0x3673–0x3676

13940–13943

R

DATETIME

Timestamp for the last input change counter preset/reset

Valid if input signal type is normal digital input.

0x3677–0x3678

13944–13945

R

INT32U

0–4294967294

Number of pulses received

Valid if input signal type is pulse digital input.

0x3679–0x367C

13946–13949

R

INT64

Resettable value of consumption

Value = pulse weight x number of pulses received

Valid if input signal type is pulse digital input.

0x367D–0x3680

13950–13953

R

INT64

Accumulated non-resettable value of consumption

Valid if input signal type is pulse digital input.

0x3681–0x3684

13954–13957

R

DATETIME

Timestamp of last resettable consumption value reset

Valid if input signal type is pulse digital input.

0x3685–0x3686

13958–13959

R

W

FLOAT32

Power calculation

Valid if

  • Input signal type is pulse digital input

  • the pulse input is from Energy pulse counter

0x3687–0x369E

13960–13983

R

OCTET STRING

Digital input identification coded over 45 ASCII characters(1)

0x369F–0x36A0

13984–13985

R

s

FLOAT32

0.003–1

Digital input 1 filter time

0x36A1

13986

R

INT16U

0–1

Input contact type(1)

  • 0 = NO (normally open contact, factory setting)

  • 1 = NC (normally close contact)

0x36A2

13987

R

INT16U

0–1

Input signal type(1)

  • 0 = normal digital input (factory setting)

  • 1 = pulse digital input

0x36A3

13988

R

INT16U

0–1

Pulse polarity(1)

  • 0 = low to high (factory setting)

  • 1 = high to low

Valid if input signal type is pulse digital input.

0x36A4

13989

R

INT16U

1–4

Pulse unit(1)

  • 1 = Wh (Watt-hour, factory setting)

  • 2 = VARh (Reactive Volt-Ampere hour)

  • 3 = VAh (Volt-Ampere hour)

  • 4 = m3 (cubic meters)

Valid if input signal type is pulse digital input.

0x36A5–0x36A6

13990–13991

R

FLOAT32

1–16777215

Pulse weight(1) (2)

Valid if input signal type is pulse digital input.

Factory setting = 1.0

0x36A7–0x36A8

13992–13993

R

INT32U

1–4294967294

Input counter threshold value(1)

Valid if input signal type is normal digital input.

Factory setting = 5000

0x36A9–0x36B8

13994–14009

Reserved

(1) Value set by using the EcoStruxure Power Commission software.

(2) Examples:

  • If each incoming pulse represents 125 kWh, and since consumption data must be expressed in watt-hours, the consumption pulse weight is 125,000.

  • If each incoming pulse represents 1 US gallon, and since consumption data must be expressed in cubic meters, the consumption pulse weight is 0.003785.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?