List of BCM ULP Module Commands and Error Codes
List of Commands
The following table lists the available BCM ULP module commands, their corresponding command codes and user profiles. Follow the command execution procedures accordingly Executing a Command.
Command |
Command Code |
User Profile |
---|---|---|
Open circuit breaker Open Circuit Breaker |
904 |
Administrator or Operator |
Close circuit breaker Close Circuit Breaker |
905 |
Administrator or Operator |
Enable/Inhibit close order Enable/Inhibit a Circuit Breaker Close Order |
910 |
Administrator or Operator |
Error Codes
In addition to generic error codes Result of the Command, the BCM ULP module commands generate the following error codes returned in register 8021:
Error Code |
Description |
---|---|
4759 (0x1297) |
Circuit breaker tripped. It must be reset before the command. |
4760 (0x1298) |
Circuit breaker already closed. |
4761 (0x1299) |
Circuit breaker already open. |
4763 (0x129B) |
FDM121 in local control mode. Remote commands not allowed. |
4766 (0x129E) |
Previous command still in progress. |
4767 (0x12A0) |
Inhibit close order enabled. |
4777 (0x12A9) |
Already in the asked state (valid only for enable/inhibit close order). |
Any other positive error code means an internal error.