DOCA0054EN-10

IO Module Identification

Introduction

The order and the description of the IO module identification registers for IO 2 are the same as those of IO 1.

Addresses and Registers List

The following table describes the identification addresses, and registers regarding the IO module.

IO Module

Addresses

Registers

IO 1

0x392F–0x3982

14640–14723

IO 2

0x44E7–0x453A

17640–17723

IMU Identification

Identification of the IMU can be set by using the EcoStruxure Power Commission software. When not programmed, the IMU identification registers return 0 (0x0000).

The FDM121 display displays the first 14 characters of the IMU name.

Address

Register

RW

Unit

Type

Range

Description

0x3931–0x3948

14642–14665

R

OCTET STRING

IMU name = up to 45 ASCII characters ended by the NULL character 0x00

0x3949–0x3960

14666–14689

R

OCTET STRING

IMU location = up to 45 ASCII characters ended by the NULL character 0x00

IO Hardware Revision

The hardware revision is an ASCII string using the format XXX.YYY.ZZZ with:

  • XXX = major version (000127)

  • YYY = minor version (000255)

  • ZZZ = revision number (000255)

The NULL character ends the revision number.

Address

Register

RW

Unit

Type

Range

Description

0x3961–0x3966

14690–14695

R

OCTET STRING

Hardware revision

IO Module Firmware Revision

The firmware revision is an ASCII string using the format XXX.YYY.ZZZ with:

  • XXX = major version (000127)

  • YYY = minor version (000255)

  • ZZZ = revision number (000255)

The NULL character ends the revision number.

Address

Register

RW

Unit

Type

Range

Description

0x3967–0x396C

14696–14701

R

OCTET STRING

Firmware revision

Current Date and Time

Address

Register

RW

Unit

Type

Range

Description

0x396D–0x3970

14702–14705

R

DATETIME

Current date and time of the IO module in DATETIME format, set by using the EcoStruxure Power Commission software.

Serial Number

The IO module serial number is composed of a maximum of 11 alphanumeric characters with the following format: PPYYWWDnnnn.

  • PP = plant code

  • YY = year of fabrication (0599)

  • WW = week of fabrication (0153)

  • D = day of fabrication (17)

  • nnnn = production number of the device on the day (00019999)

A read request of 6 registers is necessary to read the IO module serial number.

Address

Register

RW

Unit

Type

Range

Description

0x3971–0x397A

14706-14715

R

OCTET STRING

Serial number

0x3971

14706

R

OCTET STRING

‘PP’

0x3972

14707

R

OCTET STRING

‘05’–‘99’

‘YY’

0x3973

14708

R

OCTET STRING

‘01’–‘53’

‘WW’

0x3974

14709

R

OCTET STRING

‘10’–‘79’

‘Dn’

0x3975

14710

R

OCTET STRING

‘00’–‘99’

‘nn’

0x3976

14711

R

OCTET STRING

‘0’–‘9’

‘n’ (the NULL character ends the serial number)

Manufacturing Date and Time

Address

Register

RW

Unit

Type

Range

Description

0x397B–0x397E

14716–14719

R

DATETIME

Manufacturing date and time

Product Identification

Address

Register

RW

Unit

Type

Range

Description

0x392F

14640

R

INT16U

15150

Product identification = 15150 for the IO module

0x3930

14641

Reserved

0x397F–0x3982

14720–14723

R

OCTET STRING

Product code = ‘LV434063’

0x3D1C–0x3D3B

15645–15676

R–WC

OCTET STRING

User application name

0x3D3C–0x3D45

15677–15686

R

OCTET STRING

Vendor name = ‘Schneider Electric’

0x3D46–0x3D4D

15687–15694

R

OCTET STRING

Product range: ‘Enerlinx’

0x3D4E–0x3D5D

15695–15710

R

OCTET STRING

Device family: ‘IO device’

0x3D5E–0x3D65

15711–15718

R

OCTET STRING

Product model

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?