Energy Measurements
General Description
Energy measurements include:
-
active energy Ep
-
reactive energy Eq
-
apparent energy Es
-
active energy counted positively (EpIn) or negatively (EpOut), according to the configuration of register 3316 Power Flow Sign
-
reactive energy counted positively (EqIn) or negatively (EqOut), according to the configuration of register 3316 Power Flow Sign
-
active energy and reactive energy are accumulated according to the configuration of register 3324 (absolute mode by factory setting) Energy Accumulation Mode
The reset minimum/maximum command (command code = 46728) can reset the content of the energy measurement registers.
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
---|---|---|---|---|---|---|---|---|
0x07CF–0x07D2 |
2000–2003 |
R |
1 |
kWh |
MOD 10000 |
-1016 to +1016 |
E/P/H |
Total active energy: Ep (1) |
0x07D3–0x07D6 |
2004–2007 |
R |
1 |
kVARh |
MOD 10000 |
-1016 to +1016 |
E/P/H |
Total reactive energy: Eq (1) |
0x07D7–0x07DA |
2008–2011 |
R |
1 |
kWh |
MOD 10000 |
-1016 to +1016 |
P/H |
Active energy counted positively: EpIn |
0x07DB–0x07DE |
2012–2015 |
R |
1 |
kWh |
MOD 10000 |
-1016 to +1016 |
P/H |
Active energy counted negatively: EpOut |
0x07DF–0x07E2 |
2016–2019 |
R |
1 |
kVARh |
MOD 10000 |
-1016 to +1016 |
P/H |
Reactive energy counted positively: EqIn |
0x07E3–0x07E6 |
2020–2023 |
R |
1 |
kVARh |
MOD 10000 |
-1016 to +1016 |
P/H |
Reactive energy counted negatively: EqOut |
0x07E7–0x07EA |
2024–2027 |
R |
1 |
kVAh |
MOD 10000 |
-1016 to +1016 |
E/P/H |
Total apparent energy: Es |
(1) Total active energy and total reactive energy are always counted positively with MicroLogic E trip unit. |
-
The MicroLogic E trip unit screen displays positive values (only) up to 999 999 999 kWh. Over this value, MicroLogic E trip unit screen displays 999 999 999 kWh.
-
The MicroLogic P or H trip unit screen displays positive values up to 99 999 999 kWh. Over this value, MicroLogic P or H trip unit screen displays 0 and then 1 kWh.
-
The MicroLogic P or H trip unit screen displays negative values up to -99 999 999 kWh. Over this value, MicroLogic P or H trip unit screen displays 0 and then -1 kWh.
-
MOD10000 format is explained in the data type description.
The behavior is the same for reactive energy and apparent energy.