Circuit Breaker Status
Tripping Cause
The tripping cause register indicates the current status of the trip.
-
If the trip bit is set to 0, then the trip is not active.
-
If the trip bit is set to 1, then the trip is active.
The bit is reset as soon as the circuit breaker is closed again.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Bit |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x0289 |
650 |
R |
– |
– |
INT16U |
– |
– |
– |
Tripping cause for basic protection functions |
|
A/E/P/H |
0 |
Long-time protection Ir |
|||||||
|
P/H |
1 |
Short-time protection Isd |
|||||||
|
A/E |
1 |
Short-time protection Isd or Instantaneous-protection Ii |
|||||||
|
P/H |
2 |
Instantaneous-protection Ii |
|||||||
|
A/E/P/H |
3 |
Ground-fault protection Ig |
|||||||
|
A/P/H |
4 |
Earth-leakage protection (Vigi) |
|||||||
|
A/E/P/H |
5 |
Integrated Instantaneous protection |
|||||||
|
A/E |
6 |
Other protection |
|||||||
|
P/H |
Internal failure (temperature) |
||||||||
|
A/E/P/H |
7 |
Internal failure (overvoltage) |
|||||||
|
P/H |
8 |
Other protection (see register 651) |
|||||||
|
– |
9–14 |
Reserved |
|||||||
|
A/E/P/H |
15 |
If this bit is at 1, bits 0 to 14 are not valid. |
|||||||
|
0x028A |
651 |
R |
– |
– |
INT16U |
– |
– |
– |
Tripping cause for advanced protection functions |
|
P/H |
0 |
Current unbalance |
|||||||
|
P/H |
1 |
Overcurrent phase 1 |
|||||||
|
P/H |
2 |
Overcurrent phase 2 |
|||||||
|
P/H |
3 |
Overcurrent phase 3 |
|||||||
|
P/H |
4 |
Overcurrent on neutral |
|||||||
|
P/H |
5 |
Undervoltage |
|||||||
|
P/H |
6 |
Overvoltage |
|||||||
|
P/H |
7 |
Voltage unbalance |
|||||||
|
P/H |
8 |
Overpower |
|||||||
|
P/H |
9 |
Reverse power |
|||||||
|
P/H |
10 |
Underfrequency |
|||||||
|
P/H |
11 |
Overfrequency |
|||||||
|
P/H |
12 |
Phase rotation |
|||||||
|
P/H |
13 |
Load shedding based on current |
|||||||
|
P/H |
14 |
Load shedding based on power |
|||||||
|
– |
15 |
If this bit is at 1, bits 0 to 14 are not valid. |
Inhibit Close Order
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Bit |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x0291 |
658 |
R |
– |
– |
INT16U |
– |
A/E/P/H |
– |
Validity of each bit in the inhibit close order status register |
|
0x0292 |
659 |
R |
– |
– |
INT16U |
– |
A/E/P/H |
– |
Inhibit close order status |
|
0 |
Inhibit close order activated by IO module |
||||||||
|
1 |
Inhibit close order activated by remote controller |
||||||||
|
2–15 |
Reserved |
Local/Remote Mode
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x0293 |
660 |
R |
– |
– |
INT16U |
0–1 |
A/E/P/H |
Mode selected in FDM121 or IO: 0 = Remote mode (factory setting) 1 = Local mode |
Circuit Breaker Status
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Bit |
Description |
|---|---|---|---|---|---|---|---|---|---|
|
0x0294 |
661 |
R |
– |
– |
INT16U |
– |
A/E/P/H |
– |
Circuit breaker status register |
|
0 |
OF status indication contact 0 = The circuit breaker is open. 1 = The circuit breaker is closed. |
||||||||
|
1 |
SD trip indication contact 0 = Circuit breaker is not tripped. 1 = Circuit breaker is tripped due to electrical default or shunt trip or push-to-trip. Bit always equal to 0 for MasterPact and ComPact NS circuit breakers with motor mechanism. |
||||||||
|
2 |
SDE fault trip indication contact 0 = Circuit breaker is not tripped on electrical default. 1 = Circuit breaker is tripped due to electrical fault (including ground-fault test and earth-leakage test). |
||||||||
|
3 |
CH spring charged contact (only with MasterPact 0 = Spring discharged 1 = Spring charged Bit always equal to 0 for ComPact NS circuit breaker. |
||||||||
|
4 |
Reserved |
||||||||
|
5 |
PF ready to close contact (only with MasterPact) circuit breakers 0 = Not ready to close 1 = Ready to close Bit always equal to 0 for ComPact NS circuit breakers. |
||||||||
|
6 |
Distinction between ComPact NS and MasterPact NT/NW circuit breakers 0 = ComPact NS 1 = MasterPact NT/NW |
||||||||
|
7 |
Distinction between ComPact NS circuit breaker and ComPact NS circuit breaker with motor mechanism 0 = ComPact NS 1 = ComPact NS with motor mechanism |
||||||||
|
8–15 |
Reserved |
Auto/Manu
This register displays the actual mode used: Auto/Manu. These modes can be modified only locally through the HMI of MicroLogic P/H trip unit.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x029D |
670 |
R |
– |
– |
INT16 |
0…1 |
A/E/P/H |
0 = Manu: opening and closing of the circuit breaker via the communication are disabled. 1 = Auto: opening and closing of the circuit breaker via the communication are enabled (factory setting). |
Legacy Dataset Activation
Legacy dataset is available only if the BCM ULP module firmware version is greater or equal to V2.0.0 (register 577 must be greater or equal to 2000).
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x031F |
800 |
RW |
– |
– |
– |
0…1 |
A/E/P/H |
Legacy dataset activation 0 = Not activated 1 = Activated Factory setting = 0 if firmware version smaller than V3.0.0 Factory setting = 1 if firmware version greater or equal to V3.0.0 |
Communication Parameter
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x0325 |
806 |
RW |
– |
– |
– |
0–1 |
A/E/P/H |
4 Wire / 2 Wire + ULP communication parameter 0 = 4 Wire 1 = 2 Wire + ULP Factory setting = 0 if BCM ULP module firmware version smaller than V4.0.0 Factory setting = 1 if BCM ULP module firmware version greater or equal to V4.0.0 |
Energy Reduction Maintenance Switch (ERMS)
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x0326 |
807 |
R |
– |
– |
INT16U |
– |
P/H |
ERMS mode register validity: validity of each bit of the ERMS mode register. 0 = Invalid 1 = Valid |
|
0x0327 |
808 |
R |
– |
– |
INT16U |
– |
P/H |
ERMS mode: Bit 0 = 0: ERMS mode OFF Bit 0 = 1: ERMS mode ON Bit 1 = 0: ERMS not degraded mode Bit 1 = 1: ERMS degraded mode |
|
0x0328–0x0329 |
809–810 |
R |
– |
A |
INT32U |
2 x In–15 x In (limited to Ii settings) |
P/H |
ERMS setting: pickup value for ERMS setting 2 x In up to present Ii (instantaneous pickup current) setting. Factory setting = 2 x In |
|
0x032A–0x032B |
811–812 |
R |
– |
– |
– |
– |
– |
Reserved |
Contact Wear
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x032C |
813 |
R |
– |
– |
INT16U |
0–300 |
P/H |
Contact wear threshold |