Circuit Breaker Control Commands
Open Circuit Breaker
To open the circuit breaker, the user must set up the command registers the following way:
Address |
Register |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
---|---|---|---|---|---|---|---|
0x1F3F |
8000 |
– |
– |
INT16U |
904 |
A/E/P/H |
Command code = 904 |
0x1F40 |
8001 |
– |
– |
INT16U |
10 |
A/E/P/H |
Number of parameters (bytes) = 10 |
0x1F41 |
8002 |
– |
– |
INT16U |
4609 |
A/E/P/H |
Destination = 4609 (0x1201) |
0x1F42 |
8003 |
– |
– |
INT16U |
1 |
A/E/P/H |
Security type of the command |
0x1F43–0x1F44 |
8004–8005 |
– |
– |
OCTET STRING |
– |
A/E/P/H |
Password of the command: Administrator or Operator user profile password |
Close Circuit Breaker
To close the circuit breaker, the user must set up the command registers the following way:
Address |
Register |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
---|---|---|---|---|---|---|---|
0x1F3F |
8000 |
– |
– |
INT16U |
905 |
A/E/P/H |
Command code = 905 |
0x1F40 |
8001 |
– |
– |
INT16U |
10 |
A/E/P/H |
Number of parameters (bytes) = 10 |
0x1F41 |
8002 |
– |
– |
INT16U |
4609 |
A/E/P/H |
Destination = 4609 (0x1201) |
0x1F42 |
8003 |
– |
– |
INT16U |
1 |
A/E/P/H |
Security type of the command |
0x1F43–0x1F44 |
8004–8005 |
– |
– |
OCTET STRING |
– |
A/E/P/H |
Password of the command: Administrator or Operator user profile password |
Enable/Inhibit a Circuit Breaker Close Order
To enable or inhibit a close order of the circuit breaker, the user must set up the command register the following way:
Address |
Register |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
---|---|---|---|---|---|---|---|
0x1F3F |
8000 |
– |
– |
INT16U |
910 |
A/E/P/H |
Command code = 910 |
0x1F40 |
8001 |
– |
– |
INT16U |
13 |
A/E/P/H |
Number of parameters (bytes) = 13 |
0x1F41 |
8002 |
– |
– |
INT16U |
4609 |
A/E/P/H |
Destination = 4609 (0x1201) |
0x1F42 |
8003 |
– |
– |
INT16U |
1 |
A/E/P/H |
Security type of the command |
0x1F43–0x1F44 |
8004–8005 |
– |
– |
OCTET STRING |
– |
A/E/P/H |
Password of the command: Administrator or Operator user profile password |
0x1F45 |
8006 |
– |
– |
INT16U |
1 |
A/E/P/H |
|
0x1F46 |
8007 |
– |
– |
INT16U |
– |
A/E/P/H |
Origin of the command: 256 = command sent via communication interface (IFM or IFE interface) |