DOCA0054EN-10

Analog Predefined Alarms

General Description

The EcoStruxure Power Commission software enables the configuration of analog predefined alarms.

Analog predefined alarms:

  • may be modified via the command interface in configuration mode

  • are only available with a MicroLogic H trip unit

  • can be used to trigger waveform capture

Analog Predefined Alarms Number

The following table describes the list of predefined alarms and corresponding numbers, registers, and addresses.

Alarm Number

Alarm Addresses

Alarm Registers

Alarm Description

1

0x176F–0x177A

6000–6011

Overcurrent phase 1

2

0x177B–0x1786

6012–6023

Overcurrent phase 2

3

0x1787–0x1792

6024–6035

Overcurrent phase 3

4

0x1793–0x179E

6036–6047

Over neutral current

5

0x179F–0x17AA

6048–6059

Over ground current

6

0x17AB–0x17B6

6060–6071

Undercurrent phase 1

7

0x17B7–0x17C2

6072–6083

Undercurrent phase 2

8

0x17C3–0x17CE

6084–6095

Undercurrent phase 3

9

0x17CF–0x17DA

6096–6107

Overcurrent unbalance phase 1

10

0x17DB–0x17E6

6108–6119

Overcurrent unbalance phase 2

11

0x17E7–0x17F2

6120–6131

Overcurrent unbalance phase 3

12

0x17F3–0x17FE

6132–6143

Overvoltage phase 1

13

0x17FF–0x180A

6144–6155

Overvoltage phase 2

14

0x180B–0x1816

6156–6167

Overvoltage phase 3

15

0x1817–0x1822

6168–6179

Undervoltage phase 1

16

0x1823–0x182E

6180–6191

Undervoltage phase 2

17

0x182F–0x183A

6192–6203

Undervoltage phase 3

18

0x183B–0x1846

6204–6215

Overvoltage unbalance phase 1

19

0x1847–0x1852

6216–6227

Overvoltage unbalance phase 2

20

0x1853–0x185E

6228–6239

Overvoltage unbalance phase 3

21

0x185F–0x186A

6240–6251

Over total apparent power

22

0x186B–0x1876

6252–6263

Over total active power

23

0x1877–0x1882

6264–6275

Over total active reverse power

24

0x1883–0x188E

6276–6287

Over total reactive power

25

0x188F–0x189A

6288–6299

Over total reactive reverse power

26

0x189B–0x18A6

6300–6311

Under total apparent power

27

0x18A7–0x18B2

6312–6323

Under total active power

28

0x18B3–0x18BE

6324–6335

Under total active reverse power

29

0x18BF–0x18CA

6336–6347

Under total reactive power

30

0x18CB–0x18D6

6348–6359

Under total reactive reverse power

31

0x18D7–0x18E2

6360–6371

Lagging true power factor

32

0x18E3–0x18EE

6372–6383

Leading true power factor

33

0x18EF–0x18FA

6384–6395

Lagging displacement power factor

34

0x18FB–0x1906

6396–6407

Leading displacement power factor

35

0x1907–0x1912

6408–6419

Over total harmonic distortion current phase 1

36

0x1913–0x191E

6420–6431

Over total harmonic distortion current phase 2

37

0x191F–0x192A

6432–6443

Over total harmonic distortion current phase 3

38

0x192B–0x1936

6444–6455

Over total harmonic distortion voltage (phase 1 to neutral)

39

0x1937–0x1942

6456–6467

Over total harmonic distortion voltage (phase 2 to neutral)

40

0x1943–0x194E

6468–6479

Over total harmonic distortion voltage (phase 3 to neutral)

41

0x194F–0x195A

6480–6491

Over total harmonic distortion voltage (phase 1 to 2)

42

0x195B–0x1966

6492–6503

Over total harmonic distortion voltage (phase 2 to 3)

43

0x1967–0x1972

6504–6515

Over total harmonic distortion voltage (phase 3 to 1)

44

0x1973–0x197E

6516–6527

Over predicted apparent power demand

45

0x197F–0x198A

6528–6539

Over predicted total active power demand

46

0x198B–0x1996

6540–6551

Over predicted total active reverse power demand

47

0x1997–0x19A2

6552–6563

Over predicted total reactive power demand

48

0x19A3–0x19AE

6564–6575

Over predicted total reactive reverse power demand

49

0x19AF–0x19BA

6576–6587

Under predicted apparent power demand

50

0x19BB–0x19C6

6588–6599

Under predicted total active power demand

51

0x19C7–0x19D2

6600–6611

Under predicted total active reverse power demand

52

0x19D3–0x19DE

6612–6623

Under predicted total reactive power demand

53

0x19DF–0x19EA

6624–6635

Under predicted total reactive reverse power demand

Analog Predefined Alarm Record

Analog predefined alarms are coded on 12 registers.

The order and the description of the analog predefined alarms are the same as that of analog predefined alarm 1:

Analog Predefined Alarm 1

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x176F

6000

RW

INT16U

H

The MSB gives the activity of the alarm:

0 = On

1 = Off

The LSB gives the priority of the alarm:

0, 1, 2, or 3.

The factory setting value is 0x0101.

Register set to 0 will not log event into the event log (file number 10) and Waveform Capture file (file number 5).

0x1770

6001

R

INT16U

1016

H

Register number which content gets in relation to the pick-up value and to the drop-out value.

The factory setting is 1016.

0x1771

6002

R

INT16U

H

Comparison mode:

The MSB indicates Pickup mode.

The LSB indicates the Dropout mode.

MSB and LSB can be set to 1, 2 or 4:

  • 1 = immediate mode (register 6003 contains the numerical value to which the monitored register is compared) (factory setting for pickup mode and dropout mode) (2)

  • 2 = direct mode (register 6003 contains the register number of the register that is in relation to the monitored register) (percentage is applied)

  • 4 = selects bit test mode (register 6003 must contain the bitmask that gets compared (AND operation) to the monitored register)

0x1772

6003

RW

1

INT16U

H

Alarm actuation pick-up value (1)

The factory setting is 0x8000.

0x1773

6004

R

100

%

INT16U

H

This register contains a numerical value that is multiplied by the content of the pickup register when Direct Mode is selected. Otherwise, register is not used.

The factory setting is 0x8000.

0x1774

6005

RW

1

s

INT16U

H

Actuation time delay

The factory setting is 0x8000.

0x1775

6006

RW

INT16U

H

Release pick-up value (1)

The factory setting is 0x8000.

0x1776

6007

R

%

INT16U

H

This register contains a numerical value that is multiplied by the content of the pickup register when Direct Mode is selected. Otherwise, register is not used.

The factory setting is 0x8000.

0x1777

6008

RW

1

s

INT16U

0–3000

H

Release time delay.

The factory setting is 0x8000.

0x1778

6009

R

INT16U

0–3

A/E

Alarm type:

0 = Over

1 = Under (factory setting)

2 = Equal

3 = Different from

5 is used for all other alarms.

0x1779

6010

RW

INT16U

H

Action associated with overrunning of the pick-up value after the time delay has run out.

Log into the Waveform Capture file (file no. 5).

Bit 9 set to 1 = action activated

The factory setting is 0.

0x177A

6011

Reserved

(1) When Immediate mode is selected, care must be taken to set this register with the same units and scale factors as the register 6001.

(2) No percentage is applied.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?