Schematics with MasterPact NT/NW and ComPact NS Circuit Breakers
General Description
Depending on the type of circuit breaker used, the IFM interface must be connected to the circuit breaker by using one of the following configurations:
-
Connection of the IFM interface to a fixed manually-operated ComPact NS circuit breaker with a BCM ULP module.
-
Connect the IFM interface to a fixed electrically-operated MasterPact NT/NW or ComPact NS circuit breaker with a BCM ULP module.
-
Connect the IFM interface to a drawout MasterPact NT/NW or ComPact NS circuit breaker with a BCM ULP module and its respective IO module.
For more information, refer to the ULP System User Guide.
ULP Connection
| NOTICE |
|---|
|
HAZARD OF EQUIPMENT DAMAGE
Failure to follow these instructions can result in equipment damage.
|
All the connection configurations require the circuit breaker BCM ULP cord. The insulated NSX cord is mandatory for system voltages greater than 480 Vac.
Connection of the IFM Interface to a Fixed Manually-Operated ComPact NS Circuit Breaker
Connection of the IFM Interface to a Fixed Electrically-Operated MasterPact NT/NW or ComPact NS Circuit Breaker
Connection of the IFM Interface to a Drawout MasterPact NT/NW or ComPact NS Circuit Breaker

A IFM Modbus-SL interface for one circuit breaker
B RJ45 ULP cord
C Circuit breaker BCM ULP cord
D Circuit breaker disconnected position contact (CD)
E Circuit breaker cradle
F BCM ULP circuit breaker communication module
G Drawout circuit breaker
H Drawout terminal block
I Circuit breaker connected position contact (CE)
J Circuit breaker test position contact (CT)
K IO input/output application module for one circuit breaker