Metering Event Log
General Description
The system stores the events that concern the metering manager (analog predefined alarms 1 to 53) in the file 10.
This file is made up of 100 records and each record is made up of nine registers.
File Header
The following table describes the file header content:
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
---|---|---|---|---|---|---|---|---|
0x1BFB |
7164 |
RW |
– |
– |
INT16U |
– |
H |
File status: 0x0000 = file disabled 0xFFFF = file enabled (factory setting) |
0x1BFC |
7165 |
R |
– |
– |
INT16U |
– |
H |
Type of file: 10 = metering event log |
0x1BFD |
7166 |
R |
1 |
– |
INT16U |
– |
H |
Size of a file = 100 records |
0x1BFE |
7167 |
R |
1 |
– |
INT16U |
– |
H |
Size of a record = 9 registers |
0x1BFF |
7168 |
R |
– |
– |
INT16U |
1 |
H |
File filling mode: 0 = circular |
File Status
The following table describes the file status content:
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
---|---|---|---|---|---|---|---|---|
0x1C0B |
7180 |
R |
1 |
– |
INT16U |
– |
H |
Size of a file = 100 records |
0x1C0C |
7181 |
R |
1 |
– |
INT16U |
– |
H |
Size of a record = 9 registers |
0x1C0D |
7182 |
R |
1 |
– |
INT16U |
– |
H |
0x0000 = file OK 0x000A = record size smaller than expected 0x0014 = record size larger than expected 0x001E = insufficient memory 0x00FA = internal error 0x00FD = corrupted allocation table 0x00FE = configuration zero 0x00FF = invalid configuration 0xFC00 = invalid file number 0xFD00 = invalid record number 0xFE00 = file not supported 0xFF00 = cannot allocate file |
0x1C0E |
7183 |
R |
1 |
– |
INT16U |
0–100 |
H |
Number of records in the file |
0x1C0F |
7184 |
R |
1 |
– |
INT16U |
0–8000 |
H |
Sequence number of first record in the file (the oldest) |
0x1C10 |
7185 |
R |
1 |
– |
INT16U |
0–8000 |
H |
Sequence number of last record in the file (the most recent) |
0x1C11– 0x1C13 |
7186– 7188 |
R |
– |
– |
DATE |
– |
H |
Date the last file was reset. Factory setting = 0x8000 0x8000 0x8000 |
Metering Event Record
The following table shows the format of one record in the metering log:
Registers |
Type |
Bits |
Description |
---|---|---|---|
1–4 |
XDATE |
– |
Event date |
5 |
INT16U |
– |
Event number: analog predefined alarms 1–53 |
6 |
INT16U |
– |
Extreme value |
7 |
INT16U |
0–7 |
1 = alarm of the over type 2 = alarm of the under type 3 = alarm of the equal to type 4 = alarm of the different from type 5 = all other alarms |
8–11 |
1 = start of an alarm 2 = end of an alarm |
||
12–15 |
Alarms 1100–1106 have a priority 3. For other alarms, the value contained in these 4 bits represents the priority linked to the event (if applicable and depending on the alarm configuration). |
||
8 |
INT16U |
– |
Logging register associated to the alarm (1) |
9 |
INT16U |
– |
Action register associated to the alarm (1) |
(1) Registers 8 and 9 are a copy of the alarm configuration registers at the moment the event occurred. These registers depend entirely on the user configurations. For the events 1100–1106, these registers are forced to 32768. |