DOCA0054EN-10

Status

Predefined Alarms Status

The predefined alarms status register indicates the current status of the alarms:

  • alarm bit = 0: alarm is not active.

  • alarm bit = 1: alarm is active.

The following table details the values for each bit of the alarm status registers:

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Bit

Description

0x1643

5700

R

INT16U

H

Predefined alarms status

0

Predefined alarm 48

1

Predefined alarm 49

2

Predefined alarm 50

3

Predefined alarm 51

4

Predefined alarm 52

5

Predefined alarm 53

6

Predefined alarm 54

7

Predefined alarm 55

8

Predefined alarm 56

9

Predefined alarm 57

10

Predefined alarm 58

11

Predefined alarm 59

12

Predefined alarm 60

13

Predefined alarm 61

14

Predefined alarm 62

15

Predefined alarm 63

0x1644

5701

R

INT16U

H

Predefined alarms status

0

Predefined alarm 32

1

Predefined alarm 33

2

Predefined alarm 34

3

Predefined alarm 35

4

Predefined alarm 36

5

Predefined alarm 37

6

Predefined alarm 38

7

Predefined alarm 39

8

Predefined alarm 40

9

Predefined alarm 41

10

Predefined alarm 42

11

Predefined alarm 43

12

Predefined alarm 44

13

Predefined alarm 45

14

Predefined alarm 46

15

Predefined alarm 47

0x1645

5702

R

INT16U

H

Predefined alarms status

0

Predefined alarm 16

1

Predefined alarm 17

2

Predefined alarm 18

3

Predefined alarm 19

4

Predefined alarm 20

5

Predefined alarm 21

6

Predefined alarm 22

7

Predefined alarm 23

8

Predefined alarm 24

9

Predefined alarm 25

10

Predefined alarm 26

11

Predefined alarm 27

12

Predefined alarm 28

13

Predefined alarm 29

14

Predefined alarm 30

15

Predefined alarm 31

0x1646

5703

R

INT16U

H

Predefined alarms status

0

Predefined alarm 0

1

Predefined alarm 1

2

Predefined alarm 2

3

Predefined alarm 3

4

Predefined alarm 4

5

Predefined alarm 5

6

Predefined alarm 6

7

Predefined alarm 7

8

Predefined alarm 8

9

Predefined alarm 9

10

Predefined alarm 10

11

Predefined alarm 11

12

Predefined alarm 12

13

Predefined alarm 13

14

Predefined alarm 14

15

Predefined alarm 15

M2C/M6C Programmable Contacts Status

The M2C/M6C status register indicates the status of the programmable contacts:

  • status bit = 0: the contact is open.

  • status bit = 1: the contact is closed.

The contact statuses are automatically updated, a reset is not possible.

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Bit

Description

0x2298

8857

R

INT16U

E/P/H

0

Contact 1 status

E/P/H

1

Contact 2 status

P/H

2

Contact 3 status

P/H

3

Contact 4 status

P/H

4

Contact 5 status

P/H

5

Contact 6 status

6–15

Reserved

Protection Status

The following table details the values for each bit of protection pick-up value registers:

  • protection status bit = 0: protection pick-up value is not overrun.

  • protection status bit = 1: protection pick-up value is overrun, even if the time delay has not expired.

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Bit

Description

0x229D

8862

R

INT16U

E/P/H

0

Long-time protection status

1–15

Reserved

0x229E

8863

R

INT16U

P/H

0

Current-unbalance status

1

Maximum current status on phase 1

2

Maximum current status on phase 2

3

Maximum current status on phase 3

4

Maximum current status on the neutral

5

Minimum voltage status

6

Maximum voltage status

7

Voltage unbalance status

8

Maximum power status

9

Reverse power status

10

Minimum frequency status

11

Maximum frequency status

12

Phase rotation status

13

Load shedding based on current status

14

Load shedding based on power status

15

Reserved

0x229F

8864

R

INT16U

E/P/H

0

Ground-fault alarm status

P/H

1

Earth-leakage alarm status

2–15

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?