Minimum/Maximum Values of Real-Time Measurements
Minimum/Maximum Measurements Rule
Minimum and maximum measurements take into account the relative value of real-time measurements. Therefore the following rule applies:
-3800<-400<0<200<600.
In this case:
-
the minimum value = -3800
-
the maximum value = 600
-
PFmax (or cosϕ max.) is obtained for the smallest positive value of PF (or cosϕ).
-
PFmin (or cosϕ min.) is obtained for the highest negative value of PF (or cosϕ).
The reset minimum/maximum command (command code = 46728) can reset the content of the minimum/maximum real-time measurement registers.
Minimum of Real-Time Measurements
Registers 1300 to 1599 hold the minimum values of real-time metering parameters:
-
Available only with MicroLogic E,P, and H trip units.
-
The register of the minimum value of a real-time metering parameter is equal to the register of the real-time metering parameter plus 300.
Examples:
-
Register 1300 holds the minimum value of the phase-to-phase voltage V12 (register 1000).
-
Register 1316 holds the minimum value of the current on phase 1 (register 1016).
-
-
The order of the registers is the same as that of the real-time metering variables.
-
The scale factors of the minimum values are the same as those of the real-time metering parameters.
-
The minimum values of arithmetic means and unbalance voltage (registers 1306–1315) and for unbalance current (registers 1327 to 1332) are not available with MicroLogic E trip units.
Maximum of Real-Time Measurements
Registers 1600 to 1899 hold the maximum values of real-time metering parameters:
-
Available only with MicroLogic E,P, and H trip units.
-
The register of the maximum value of a real-time metering parameter is equal to the register of the real-time metering parameter plus 600.
Examples:
-
Register 1600 holds the maximum value of the phase-to-phase voltage V12 (register 1000).
-
Register 1616 holds the maximum value of the current on phase 1 (register 1016).
-
-
The order of the registers is the same as that of the real-time metering variables.
-
The scale factors of the maximum values are the same as those of the real-time metering parameters.
-
The maximum values of arithmetic means and unbalance voltage (registers 1606–1615) and for unbalance current (registers 1627 to 1632) are not available with MicroLogic E trip units.