BCM ULP Module Identification
Product Identification
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
---|---|---|---|---|---|---|---|---|
0x0202 |
515 |
R |
– |
– |
INT16U |
15139 |
A/E/P/H |
Product identification = 15139 for the BCM ULP module |
BCM ULP Module Identifier
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
---|---|---|---|---|---|---|---|---|
0x0215–0x0216 |
534–535 |
RW |
– |
– |
OCTET STRING |
0x0000–0x7F7F |
A/E/P/H |
Short identifier of BCM ULP module coded over 4 ASCII characters Factory setting = 0x0000 |
0x0217–0x021E |
536–543 |
RW |
– |
– |
OCTET STRING |
0x0000–0x7F7F |
A/E/P/H |
Long identifier of BCM ULP module coded over 16 ASCII characters Factory setting = 0x0000 |
BCM ULP Module Firmware Version
The BCM ULP module firmware version starts with a V character and has the following format: VX.Y.Z.
The firmware version is coded as follows: VX.Y.Z = VX*1000 + Y*100 + Z*10
For example if the value of the register is equal to 2000, the BCM ULP module firmware version is equal to V2.0.0.
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
---|---|---|---|---|---|---|---|---|
0x0240 |
577 |
R |
– |
– |
INT16U |
– |
A/E/P/H |
BCM ULP module firmware version |