DOCA0054EN-10

Miscellaneous

Nominal Current

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x222D

8750

R

1

A

INT16U

0–8000

A/E/P/H

Rated circuit breaker current

Factory setting = 100 A (circuit breaker sensor plug not present)

Protection Manager Measurements

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x2263

8804

R

INT16U

0–65535

P/H

Protection Manager (PM) configuration change counter

This counter is incremented each time a PM setting change is applied through HMI (keyboard or switches) or COM.

If switches were changed during power off, this counter is incremented at power-up.

0x2280

8833

R

10

%In

INT16U

0–16000

P/H

Maximum fault current (trip) recorded on phase 1 since last reset (4)

Factory setting = 0x8000 (no fault recorded or circuit breaker type not entered)

0x2281

8834

R

10

%In

INT16U

0–16000

P/H

Maximum fault current (trip) recorded on phase 2 since last reset (4)

Factory setting = 0x8000 (no fault recorded or circuit breaker type not entered)

0x2282

8835

R

10

%In

INT16U

0–16000

P/H

Maximum fault current (trip) recorded on phase 3 since last reset (4)

Factory setting = 0x8000 (no fault recorded or circuit breaker type not entered)

0x2283

8836

R

10

%In

INT16U

0–16000

P/H

Maximum fault current (trip) recorded on the neutral since last reset (4)

Factory setting = 0x8000 (no fault recorded or circuit breaker code not supplied)

0x2284

8837

R

1

%Ir

INT16U

0–32767

A/P/H

RMS current on phase 1 expressed as a % of the Ir long-time pick-up value

0x2285

8838

R

1

%Ir

INT16U

0–32767

A/P/H

RMS current on phase 2 expressed as a % of the Ir long-time pick-up value

0x2286

8839

R

1

%Ir

INT16U

0–32767

A/P/H

RMS current on phase 3 expressed as a % of the Ir long-time pick-up value

0x2287

8840

R

1

%Ir

INT16U

0–32767

A/P/H

RMS current on the neutral expressed as a % of the rated current In x the selected neutral setting (x 1, x 2 or x 0.5) (1)

0x2288

8841

R

1

%Ig

INT16U

0–32767

A/P/H

"Residual" ground-fault current expressed as a % of the Ig ground-fault protection pick-up value (2)

0x2289

8842

R

100

%Idn

INT16U

0–32767

A/P/H

Earth-leakage current expressed as a % of the IΔN earth-leakage protection pick-up value (3)

(1) Value not accessible when configuration register 9618 selects "no external CT".

(2) Accessible only with MicroLogic 6.0 trip unit.

(3) Accessible only with MicroLogic 7.0 trip unit.

(4) Auxiliary power is required to calculate the fault currents. Calculation is effective only when the circuit breaker selection code has been supplied (see the MicroLogic P/H trip units user guides).

Battery Status

The following table represents the battery charge status:

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x228A

8843

R

1

%

INT16U

0–100

A/E/P/H

Battery-charge indicator:

100 % = U > 2800 mV

50 % = 2200 < U < 2800 mV

0 % = U < 2200 mV

Time Remaining Until Long-Time Tripping

Time remaining until long-time tripping is evaluated every second. If another protection is tripped, then time remaining until long-time tripping continues to be evaluated.

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x22A0–0x22A1

8865–8866

R

10

s

MOD 10000

P/H

Time remaining until long-time tripping

Phase Rotation

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x22A7

8872

R

INT16U

P/H

Phase rotation:

0 = ABC (123)

1 = ACB (132)

Language

This register sets the language used by the trip unit. It may be modified through the trip unit keypad. The factory setting is English but it may be factory set if necessary.

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Bit

Description

0x258D

9614

RW

INT16U

P/H

0

French

1

US English

2

UK English

3

German

4

Spanish

5

Italian

7

Chinese

8

Russian

9

Optional language available on order from Schneider Electric

10–15

Reserved

Nominal Frequency

This register rates the circuit breaker operating frequency required by the protection manager to disable phase rotation protection for 400 Hz distribution system.

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Bit

Description

0x258E

9615

RW

INT16U

P/H

0

50 / 60 Hz (factory setting)

1–2

Reserved

3

400 Hz

4–15

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?