DOCA0054EN-10

Maintenance Protection Event Log

General Description

The system stores the events that concern the maintenance protection manager (power-up, M6C programmable contacts, maximum peak fault current, and so on) in the file number 21.

This file is made up of 20 records and each record is made up of six registers.

This maintenance event log has been implemented on MicroLogic P trip unit with firmware Plogic2002AA and above.

File Header

The following table describes the file header content:

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x26CB

9932

RW

INT16U

H

File status:

0x0000 = file disabled

0xFFFF = file enabled (factory setting)

0x26CC

9933

R

INT16U

H

Type of file:

21 = maintenance protection event log

0x26CD

9934

R

1

INT16U

H

Size of a file = 20 records

0x26CE

9935

R

1

INT16U

H

Size of a record = 6 registers

0x26CF

9936

R

INT16U

1

H

File filling mode:

1 = disabled if log is full

File Status

The following table describes the file status content:

Address

Register

RW

X

Unit

Type

Range

A/E/P/H

Description

0x26DB

9948

R

1

INT16U

H

Size of a file = 20 records

0x26DC

9949

R

1

INT16U

H

Size of a record = 6 registers

0x26DD

9950

R

1

INT16U

H

0x0000 = file OK

0x000A = record size smaller than expected

0x0014 = record size larger than expected

0x001E = insufficient memory

0x00FA = internal error

0x00FD = corrupted allocation table

0x00FE = configuration zero

0x00FF = invalid configuration

0xFC00 = invalid file number

0xFD00 = invalid record number

0xFE00 = file not supported

0xFF00 = cannot allocate file

0x26DE

9951

R

1

INT16U

20

H

Number of records in the file = 20

0x26DF

9952

R

1

INT16U

1

P/H

Sequence number of first record in the file (the oldest) = 1

0x26E0

9953

R

1

INT16U

20

P/H

Sequence number of last record in the file (the most recent) = 20

0x26E1– 0x26E3

9954– 9956

R

DATE

H

Date the last file was reset.

Factory setting = 0x8000 0x8000 0x8000

Maintenance Protection Event Record

The maintenance protection event log has a fixed number of records and all record has a fixed number of registers:

Record Number

Registers

Type

Description

1

1–4

XDATE

Last power loss

5–6

Reserved

2

1–3

DATE

Date/time of last counter reset

4

INT16U

Number of output operations for relay 1

5–6

Reserved

3–6

1–3

DATE

Date/time of last counter reset

4

INT16U

Number of output operations for relay 2–5

5–6

Reserved

7

1–3

DATE

Date/time of last counter reset

4

INT16U

Number of output operations for relay 6

5–6

Reserved

8

1–3

DATE

Date/time of last record updated

4

INT16U

Worst contact wear

5–6

Reserved

9

1–3

DATE

Date/time of last record updated

4

INT16U

Maximum reverse power

5–6

Reserved

10

1–3

DATE

Date/time of last record updated

4

INT16U

Battery indicator

5–6

Reserved

11

1–3

DATE

Date/time of last record updated

4

INT16U

Number of power losses

5–6

Reserved

12–15

1–6

Reserved

16

1–3

DATE

Date/time of last record updated

4

INT16U

Number of maximum resets

5–6

Reserved

17

1–6

Reserved

18

1–3

DATE

Date/time of last record updated

4

INT16U

Maximum peak fault current breaker ever opened

5–6

Reserved

19–20

1–6

Reserved

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?