Real-Time Measurements
General Description
The metering manager refreshes the real-time measurements every second. Real-time measurements include:
-
voltage and voltage unbalance
-
current and current unbalance
-
active, reactive, apparent, and distortion power
-
power factor and fundamental power factor
-
frequency
-
fundamental voltage and current
-
fundamental active, reactive, and apparent power
-
THD (total harmonic distortion in relation to the fundamental)
-
thd (total harmonic distortion in relation to the RMS value)
-
voltage to current phase shift
-
K-factor
-
peak factor
-
voltage to voltage phase shift
Voltage
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x03E7 |
1000 |
R |
1 |
V |
INT16U |
0–1200 |
E/P/H |
RMS phase-to-phase voltage V12 |
|
0x03E8 |
1001 |
R |
1 |
V |
INT16U |
0–1200 |
E/P/H |
RMS phase-to-phase voltage V23 |
|
0x03E9 |
1002 |
R |
1 |
V |
INT16U |
0–1200 |
E/P/H |
RMS phase-to-phase voltage V31 |
|
0x03EA |
1003 |
R |
1 |
V |
INT16U |
0–1200 |
E/P/H |
RMS phase-to-neutral voltage V1N (1) |
|
0x03EB |
1004 |
R |
1 |
V |
INT16U |
0–1200 |
E/P/H |
RMS phase-to-neutral voltage V2N (1) |
|
0x03EC |
1005 |
R |
1 |
V |
INT16U |
0–1200 |
E/P/H |
RMS phase-to-neutral voltage V3N (1) |
|
0x03ED |
1006 |
R |
1 |
V |
INT16U |
0–1200 |
E/P/H |
Arithmetic mean of V12, V23, and V31: (V12 + V23 + V31) / 3 = Vavg L-L |
|
0x03EE |
1007 |
R |
1 |
V |
INT16U |
0–1200 |
E/P/H |
Arithmetic mean of V1N, V2N, and V3N: (V1N + V2N + V3N) / 3 = Vavg L-N (1) |
|
(1) Value is not available when the system type in register 3314 is 30 or 31. Refer to System Type. |
||||||||
Voltage Unbalance
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x03EF |
1008 |
R |
10 |
% |
INT16 |
-1000–+1000 |
E/P/H |
V12 phase-to-phase voltage unbalance in relation to the arithmetic mean of phase-to-phase voltages |
|
0x03F0 |
1009 |
R |
10 |
% |
INT16 |
-1000–+1000 |
E/P/H |
V23 phase-to-phase voltage unbalance in relation to the arithmetic mean of phase-to-phase voltages |
|
0x03F1 |
1010 |
R |
10 |
% |
INT16 |
-1000–+1000 |
E/P/H |
V31 phase-to-phase voltage unbalance in relation to the arithmetic mean of phase-to-phase voltages |
|
0x03F2 |
1011 |
R |
10 |
% |
INT16 |
-1000–+1000 |
E/P/H |
V1N phase-to-neutral voltage unbalance in relation to the arithmetic mean of phase-to-neutral voltages (1) |
|
0x03F3 |
1012 |
R |
10 |
% |
INT16 |
-1000–+1000 |
E/P/H |
V2N phase-to-neutral voltage unbalance in relation to the arithmetic mean of phase-to-neutral voltages (1) |
|
0x03F4 |
1013 |
R |
10 |
% |
INT16 |
-1000–+1000 |
E/P/H |
V3N phase-to-neutral voltage unbalance in relation to the arithmetic mean of phase-to-neutral voltages (1) |
|
0x03F5 |
1014 |
R |
10 |
% |
INT16 |
-1000–+1000 |
E/P/H |
Maximum phase-to-phase voltage unbalance value of registers 1008, 1009, and 1010 |
|
0x03F6 |
1015 |
R |
10 |
% |
INT16 |
-1000–+1000 |
E/P/H |
Maximum phase-to-neutral voltage unbalance value of registers 1011, 1012, and 1013 (1) |
|
(1) Value is not available when the system type in register 3314 is 30 or 31. Refer to System Type. |
||||||||
Current
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x03F7 |
1016 |
R |
1 |
A |
INT16U |
0–32767 |
A/E/P/H |
RMS current on phase 1: I1 |
|
0x03F8 |
1017 |
R |
1 |
A |
INT16U |
0–32767 |
A/E/P/H |
RMS current on phase 2: I2 |
|
0x03F9 |
1018 |
R |
1 |
A |
INT16U |
0–32767 |
A/E/P/H |
RMS current on phase 3: I3 |
|
0x03FA |
1019 |
R |
1 |
A |
INT16U |
0–32767 |
A/E/P/H |
RMS current on the neutral: IN (1) |
|
0x03FB |
1020 |
R |
1 |
A |
INT16U |
0–32767 |
A/E/P/H |
Maximum of I1, I2, I3, and IN |
|
0x03FC |
1021 |
R |
1 |
%lg |
INT16U |
0–32767 |
A/E/P/H |
Ground-fault current (2) |
|
0x03FD |
1022 |
R |
1 |
mA |
INT16U |
0–32767 |
A/P/H |
Earth-leakage current(3)(4) |
|
0x03FE |
1023 |
R |
1 |
A |
INT16U |
0–32767 |
H |
Apparent current phase 1 (peak/√2) |
|
0x03FF |
1024 |
R |
1 |
A |
INT16U |
0–32767 |
H |
Apparent current phase 2 (peak/√2) |
|
0x0400 |
1025 |
R |
1 |
A |
INT16U |
0–32767 |
H |
Apparent current phase 3 (peak/√2) |
|
0x0401 |
1026 |
R |
1 |
A |
INT16U |
0–32767 |
H |
Apparent current neutral (peak/√2) |
|
0x0402 |
1027 |
R |
1 |
A |
INT16U |
0–32767 |
E/P/H |
Arithmetic mean of I1, I2, and I3: (I1 + I2 + I3) / 3 = Iavg |
|
(1) Value is not available when the system type in register 3314 is 31 or 40. Refer to System Type. (2) Accessible only with MicroLogic 5.0 P/H and 6.0 A/E/P/H trip units. (3) Accessible only with MicroLogic 7.0 A/P/H trip units. (4) If this current exceeds 32767 A, the register blocks at 32767. |
||||||||
Current Unbalance
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x0403 |
1028 |
R |
10 |
% |
INT16 |
-1000–+1000 |
E/P/H |
I1 current unbalance in relation to the arithmetic mean of the phase currents |
|
0x0404 |
1029 |
R |
10 |
% |
INT16 |
-1000–+1000 |
E/P/H |
I2 current unbalance in relation to the arithmetic mean of the phase currents |
|
0x0405 |
1030 |
R |
10 |
% |
INT16 |
-1000–+1000 |
E/P/H |
I3 current unbalance in relation to the arithmetic mean of the phase currents |
|
0x0406 |
1031 |
R |
10 |
% |
INT16 |
-1000–+1000 |
E/P/H |
IN current unbalance in relation to the arithmetic mean of the phase currents (1) |
|
0x0407 |
1032 |
R |
10 |
% |
INT16 |
-1000–+1000 |
E/P/H |
Maximum current unbalance of registers 1028, 1029, and 1030 |
|
(1) Value is not available when the system type in register 3314 is 31 or 40. Refer to System Type. |
||||||||
Active Power
The flow sign of the active power depends on the configuration of register 3316.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x0409 |
1034 |
R |
1 |
kW |
INT16 |
-32767–+32767 |
E/P/H |
Active power on phase 1: P1 (1) |
|
0x040A |
1035 |
R |
1 |
kW |
INT16 |
-32767–+32767 |
E/P/H |
Active power on phase 2: P2 (1) |
|
0x040B |
1036 |
R |
1 |
kW |
INT16 |
-32767–+32767 |
E/P/H |
Active power on phase 3: P3 (1) |
|
0x040C |
1037 |
R |
1 |
kW |
INT16 |
-32767–+32767 |
E/P/H |
Total active power: Ptot |
|
(1) Value is not available when the system type in register 3314 is 30 or 31. Refer to System Type. |
||||||||
Reactive Power
The flow sign of the reactive power depends on the configuration of register 3316.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x040D |
1038 |
R |
1 |
kVAR |
INT16 |
-32767–+32767 |
E/P/H |
Reactive power on phase 1: Q1 |
|
0x040E |
1039 |
R |
1 |
kVAR |
INT16 |
-32767–+32767 |
E/P/H |
Reactive power on phase 2: Q2 |
|
0x040F |
1040 |
R |
1 |
kVAR |
INT16 |
-32767–+32767 |
E/P/H |
Reactive power on phase 3: Q3 |
|
0x0410 |
1041 |
R |
1 |
kVAR |
INT16 |
-32767–+32767 |
E/P/H |
Total reactive power: Qtot |
|
(1) Value is not available when the system type in register 3314 is 30 or 31. Refer to System Type. |
||||||||
Apparent Power
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x0411 |
1042 |
R |
1 |
kVA |
INT16U |
0–32767 |
E/P/H |
Apparent power on phase 1: S1 (1) |
|
0x0412 |
1043 |
R |
1 |
kVA |
INT16U |
0–32767 |
E/P/H |
Apparent power on phase 2: S2 (1) |
|
0x0413 |
1044 |
R |
1 |
kVA |
INT16U |
0–32767 |
E/P/H |
Apparent power on phase 3: S3 (1) |
|
0x0414 |
1045 |
R |
1 |
kVA |
INT16U |
0–32767 |
E/P/H |
Total apparent power: Stot |
|
(1) Value is not available when the system type in register 3314 is 30 or 31. Refer to System Type. |
||||||||
Power Factor
The sign of the power factor depends on the configuration of register 3318.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x0415 |
1046 |
R |
1000 |
– |
INT16 |
-1000–+1000 |
E/P/H |
Power factor on phase 1: PF1 (absolute value equal to |P1|/S1) (1) |
|
0x0416 |
1047 |
R |
1000 |
– |
INT16 |
-1000–+1000 |
E/P/H |
Power factor on phase 2: PF2 (absolute value equal to |P2|/S2) (1) |
|
0x0417 |
1048 |
R |
1000 |
– |
INT16 |
-1000–+1000 |
E/P/H |
Power factor on phase 3: PF3 (absolute value equal to |P3|/S3) (1) |
|
0x0418 |
1049 |
R |
1000 |
– |
INT16 |
-1000–+1000 |
E/P/H |
Total power factor: PF (absolute value equal to |Ptotal| / Stotal) (1) |
|
(1) Value is not available when the system type in register 3314 is 30 or 31. Refer to System Type. |
||||||||
Fundamental Power Factor (cosϕ)
The sign of the fundamental power factor (cosϕ) depends on the configuration of register 3318.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x0419 |
1050 |
R |
1000 |
– |
INT16 |
-1000–+1000 |
H |
Fundamental power factor on phase 1: cosϕ1 (absolute value equal to |P1 Fund|/S1 Fund) (1) |
|
0x041A |
1051 |
R |
1000 |
– |
INT16 |
-1000–+1000 |
H |
Fundamental power factor on phase 2: cosϕ2 (absolute value equal to |P2 Fund|/S2 Fund) (1) |
|
0x041B |
1052 |
R |
1000 |
– |
INT16 |
-1000–+1000 |
H |
Fundamental power factor on phase 3: cosϕ3 (absolute value equal to |P3 Fund|/S3 Fund) (1) |
|
0x041C |
1053 |
R |
1000 |
– |
INT16 |
-1000–+1000 |
H |
Total fundamental power factor: cosφ (absolute value equal to |Ptot Fund|/Stot Fund) |
|
(1) Value is not available when the system type in register 3314 is 30 or 31. Refer to System Type. |
||||||||
Frequency
When the MicroLogic trip unit cannot calculate the frequency, it returns Not applicable = 32768 (0x8000).
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x041D |
1054 |
R |
10 |
Hz |
INT16U |
400–600 |
P/H |
System frequency: F |
Fundamental Voltage
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x041F |
1056 |
R |
1 |
V |
INT16U |
0–1200 |
H |
Fundamental rms phase-to-phase voltage V12 Fund |
|
0x0420 |
1057 |
R |
1 |
V |
INT16U |
0–1200 |
H |
Fundamental rms phase-to-phase voltage V23 Fund |
|
0x0421 |
1058 |
R |
1 |
V |
INT16U |
0–1200 |
H |
Fundamental rms phase-to-phase voltage V31 Fund |
|
0x0422 |
1059 |
R |
1 |
V |
INT16U |
0–1200 |
H |
Fundamental rms phase-to-neutral voltage V1N Fund (1) |
|
0x0423 |
1060 |
R |
1 |
V |
INT16U |
0–1200 |
H |
Fundamental rms phase-to-neutral voltage V2N Fund (1) |
|
0x0424 |
1061 |
R |
1 |
V |
INT16U |
0–1200 |
H |
Fundamental rms phase-to-neutral voltage V3N Fund (1) |
|
(1) Value is not available when the system type in register 3314 is 30 or 31. Refer to System Type. |
||||||||
Fundamental Current
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x042B |
1068 |
R |
1 |
A |
INT16U |
0–32767 |
H |
Fundamental rms current on phase 1: I1 Fund |
|
0x042C |
1069 |
R |
1 |
A |
INT16U |
0–32767 |
H |
Fundamental rms current on phase 2: I2 Fund |
|
0x042D |
1070 |
R |
1 |
A |
INT16U |
0–32767 |
H |
Fundamental rms current on phase 3: I3 Fund |
|
0x042E |
1071 |
R |
1 |
A |
INT16U |
0–32767 |
H |
Fundamental rms current on neutral: IN Fund (1) (2) |
|
(1) Value is not available when the system type in register 3314 is 31 or 40. Refer to System Type. (2) Measured with system type 41. |
||||||||
Fundamental Active Power
The flow sign of the active power depends on the configuration of register 3316.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x0433 |
1076 |
R |
1 |
kW |
INT16U |
-32767–32767 |
H |
Fundamental active power on phase 1: P1 Fund (1) |
|
0x0434 |
1077 |
R |
1 |
kW |
INT16U |
-32767–32767 |
H |
Fundamental active power on phase 2: P2 Fund (1) |
|
0x0435 |
1078 |
R |
1 |
kW |
INT16U |
-32767–32767 |
H |
Fundamental active power on phase 3: P3 Fund (1) |
|
0x0436 |
1079 |
R |
1 |
kW |
INT16U |
-32767–32767 |
H |
Total fundamental active power: Ptot Fund |
|
(1) Value is not available when the system type in register 3314 is 30 or 31. Refer to System Type. |
||||||||
Fundamental Reactive Power
The flow sign of the reactive power depends on the configuration of register 3316.
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x0437 |
1080 |
R |
1 |
kVAR |
INT16U |
-32767–32767 |
H |
Fundamental reactive power on phase 1: Q1 Fund (1) |
|
0x0438 |
1081 |
R |
1 |
kVAR |
INT16U |
-32767–32767 |
H |
Fundamental reactive power on phase 2: Q2 Fund (1) |
|
0x0439 |
1082 |
R |
1 |
kVAR |
INT16U |
-32767–32767 |
H |
Fundamental reactive power on phase 3: Q3 Fund (1) |
|
0x043A |
1083 |
R |
1 |
kVAR |
INT16U |
-32767–32767 |
H |
Total fundamental reactive power: Qtot Fund |
|
(1) Value is not available when the system type in register 3314 is 30 or 31. Refer to System Type. |
||||||||
Fundamental Apparent Power
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x043B |
1084 |
R |
1 |
kVA |
INT16U |
0–32767 |
H |
Fundamental apparent power on phase 1: S1 Fund (1) |
|
0x043C |
1085 |
R |
1 |
kVA |
INT16U |
0–32767 |
H |
Fundamental apparent power on phase 2: S2 Fund (1) |
|
0x043D |
1086 |
R |
1 |
kVA |
INT16U |
0–32767 |
H |
Fundamental apparent power on phase 3: S3 Fund (1) |
|
0x043E |
1087 |
R |
1 |
kVA |
INT16U |
0–32767 |
H |
Total fundamental apparent power: Stot Fund |
|
(1) Value is not available when the system type in register 3314 is 30 or 31. Refer to System Type. |
||||||||
Distortion Power
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x043F |
1088 |
R |
1 |
kVAR |
INT16U |
0–32767 |
H |
Distortion power on phase 1: D1 (1) |
|
0x0440 |
1089 |
R |
1 |
kVAR |
INT16U |
0–32767 |
H |
Distortion power on phase 2: D2 (1) |
|
0x0441 |
1090 |
R |
1 |
kVAR |
INT16U |
0–32767 |
H |
Distortion power on phase 3: D3 (1) |
|
0x0442 |
1091 |
R |
1 |
kVAR |
INT16U |
0–32767 |
H |
Total distortion power: Dtot |
|
(1) Value is not available when the system type in register 3314 is 30 or 31. Refer to System Type. |
||||||||
Total Harmonic Distortion in Relation to the Fundamental (THD)
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x0443 |
1092 |
R |
10 |
% |
INT16U |
0–5000 |
H |
Total harmonic distortion of V12 in relation to the fundamental |
|
0x0444 |
1093 |
R |
10 |
% |
INT16U |
0–5000 |
H |
Total harmonic distortion of V23 in relation to the fundamental |
|
0x0445 |
1094 |
R |
10 |
% |
INT16U |
0–5000 |
H |
Total harmonic distortion of V31 in relation to the fundamental |
|
0x0446 |
1095 |
R |
10 |
% |
INT16U |
0–5000 |
H |
Total harmonic distortion of V1N in relation to the fundamental (1) |
|
0x0447 |
1096 |
R |
10 |
% |
INT16U |
0–5000 |
H |
Total harmonic distortion of V2N in relation to the fundamental (1) |
|
0x0448 |
1097 |
R |
10 |
% |
INT16U |
0–5000 |
H |
Total harmonic distortion of V3N in relation to the fundamental (1) |
|
0x0449 |
1098 |
R |
10 |
% |
INT16U |
0–5000 |
H |
Total harmonic distortion of I1 in relation to the fundamental |
|
0x044A |
1099 |
R |
10 |
% |
INT16U |
0–5000 |
H |
Total harmonic distortion of I2 in relation to the fundamental |
|
0x044B |
1100 |
R |
10 |
% |
INT16U |
0–5000 |
H |
Total harmonic distortion of I3 in relation to the fundamental |
|
0x044C |
1101 |
R |
10 |
% |
INT16U |
0–5000 |
H |
Total harmonic distortion of IN in relation to the fundamental (1) (2) |
|
(1) Value is not available when the system type in register 3314 is 30 or 31. Refer to System Type. (2) Measured with system type 41, calculated with system type 40. |
||||||||
Total Harmonic Distortion in Relation to the RMS Value (thd)
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x044D |
1102 |
R |
10 |
% |
INT16U |
0–1000 |
H |
Total harmonic distortion of V12 in relation to the rms value |
|
0x044E |
1103 |
R |
10 |
% |
INT16U |
0–1000 |
H |
Total harmonic distortion of V23 in relation to the rms value |
|
0x044F |
1104 |
R |
10 |
% |
INT16U |
0–1000 |
H |
Total harmonic distortion of V31 in relation to the rms value |
|
0x0450 |
1105 |
R |
10 |
% |
INT16U |
0–1000 |
H |
Total harmonic distortion of V1N in relation to the rms value (1) |
|
0x0451 |
1106 |
R |
10 |
% |
INT16U |
0–1000 |
H |
Total harmonic distortion of V2N in relation to the rms value (1) |
|
0x0452 |
1107 |
R |
10 |
% |
INT16U |
0–1000 |
H |
Total harmonic distortion of V3N in relation to the rms value (1) |
|
0x0453 |
1108 |
R |
10 |
% |
INT16U |
0–1000 |
H |
Total harmonic distortion of I1 in relation to the rms value |
|
0x0454 |
1109 |
R |
10 |
% |
INT16U |
0–1000 |
H |
Total harmonic distortion of I2 in relation to the rms value |
|
0x0455 |
1110 |
R |
10 |
% |
INT16U |
0–1000 |
H |
Total harmonic distortion of I3 in relation to the rms value |
|
0x0456 |
1111 |
R |
10 |
% |
INT16U |
0–1000 |
H |
Total harmonic distortion of IN in relation to the rms value (1) (2) |
|
(1) Value is not available when the system type in register 3314 is 30 or 31. Refer to System Type. (2) Measured with system type 41, calculated with system type 40. |
||||||||
Voltage-to-Current Phase Shift
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x0457 |
1112 |
R |
10 |
Deg |
INT16U |
0–3600 |
H |
|
|
0x0458 |
1113 |
R |
10 |
Deg |
INT16U |
0–3600 |
H |
|
|
0x0459 |
1114 |
R |
10 |
Deg |
INT16U |
0–3600 |
H |
|
K-Factor
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x045A |
1115 |
R |
10 |
– |
INT16U |
0–1000 |
H |
Phase 1 K-factor(2) |
|
0x045B |
1116 |
R |
10 |
– |
INT16U |
0–1000 |
H |
Phase 2 K-factor(2) |
|
0x045C |
1117 |
R |
10 |
– |
INT16U |
0–1000 |
H |
Phase 3 K-factor(2) |
|
0x045D |
1118 |
R |
10 |
– |
INT16U |
0–1000 |
H |
Neutral K-factor (1) (2) |
|
(1) Value is not available when the system type in register 3314 is 30 or 31. Refer to System Type. (2) Not applicable in 400 Hz nominal frequency system. |
||||||||
Peak Factor
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x045E |
1119 |
R |
100 |
– |
INT16U |
0–10000 |
H |
V12 voltage peak factor(3)(4) |
|
0x045F |
1120 |
R |
100 |
– |
INT16U |
0–10000 |
H |
V23 voltage peak factor(3)(4) |
|
0x0460 |
1121 |
R |
100 |
– |
INT16U |
0–10000 |
H |
V31 voltage peak factor(3)(4) |
|
0x0461 |
1122 |
R |
100 |
– |
INT16U |
0–10000 |
H |
V1N voltage peak factor (1) (4) |
|
0x0462 |
1123 |
R |
100 |
– |
INT16U |
0–10000 |
H |
V2N voltage peak factor (1) (4) |
|
0x0463 |
1124 |
R |
100 |
– |
INT16U |
0–10000 |
H |
V3N voltage peak factor (1) (4) |
|
0x0464 |
1125 |
R |
100 |
– |
INT16U |
0–10000 |
H |
Phase 1 current peak factor(4) |
|
0x0465 |
1126 |
R |
100 |
– |
INT16U |
0–10000 |
H |
Phase 2 current peak factor(4) |
|
0x0466 |
1127 |
R |
100 |
– |
INT16U |
0–10000 |
H |
Phase 3 current peak factor(4) |
|
0x0467 |
1128 |
R |
100 |
– |
INT16U |
0–10000 |
H |
Neutral current peak factor(2)(4) |
|
(1) Value is not available when the system type in register 3314 is 30 or 31. Refer to System Type. (2) Value is not available when the system type in register 3314 is 31 or 40. Refer to System Type. (3) Value is not available when the system type in register 3314 is 40 or 41. Refer to System Type. (4) Not applicable in 400 Hz nominal frequency system. |
||||||||
Voltage-to-Voltage Phase Shift
|
Address |
Register |
RW |
X |
Unit |
Type |
Range |
A/E/P/H |
Description |
|---|---|---|---|---|---|---|---|---|
|
0x046C |
1133 |
R |
10 |
Deg |
INT16U |
0–3600 |
H |
Always equal to 0. |
|
0x046D |
1134 |
R |
10 |
Deg |
INT16U |
0–3600 |
H |
Under phase balanced conditions, equals 240 degrees. |
|
0x046E |
1135 |
R |
10 |
Deg |
INT16U |
0–3600 |
H |
Under phase balanced conditions, equals 120 degrees. |