251020_SpaceLogic_KNX_Remote_SW

Creating Subscriptions

Once you have redeemed your digital vouchers, follow these steps to create your subscriptions:

Start Subscription Creation

  • In the Redeem Voucher dialog, click Subscribe Now.

  • Alternatively, go to the Digital Vouchers tab and click:

    • Subscribe with Credits or

    • Subscribe Now next to the desired subscription type.

Select Subscription Details

  • Choose the subscription type (e.g., 1-Year, 5-Year).

  • Set the quantity you want to activate.

  • Click Continue.

Review and Customize

  • Confirm the delivery email, which corresponds to the email account of the system integrator who will connect to the customer´s installation.

  • Fill in the Subscription Reference (e.g., PO number, customer name, or project name).

Place the Order

  • Click Place Order to finalize.

  • You will receive an email confirmation once the subscription is created.

What to Expect Next

  • Subscriptions may take a few minutes to appear in your account.

  • Once active, they will be visible in the ETS or eConfigure KNX.

  • A confirmation email will notify you when the process is complete. (See more in Subscription Email Notifications.)

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.