251020_SpaceLogic_KNX_Remote_SW

Space Logic KNX Remote Subscriptions

To fully activate and utilize the SpaceLogic KNX Remote feature, you need to purchase subscriptions for the controllers you want to access.

You can purchase subscriptions in two ways:

  • Via SpaceLogic KNX Remote: Click the Purchase Subscriptions button in the top-right corner of the homepage. This redirects you to the Schneider Electric Software Shop.

  • Direct Link: Visit the Schneider Electric Software Shop directly: https://www.se.com/us/en/shop/software/.

Subscription Options

Plan

SKU

Access Duration

Controller Access

Reassignment

Use Case

Monthly

LSS9002200

30 days

1 controller

Not applicable

Trial use - Occasional access without contract

1-Year (1)

LSS9002100

365 days

1 controller

Once every 30 days

Standard maintenance contracts

1-Year (5)

LSS9002101

365 days

5 controllers

Once every 30 days

Medium-sized installations

1-Year (25)

LSS9002102

365 days

25 controllers

Once every 30 days

Larger customer base

1-Year (Unlimited)

LSS9002103

365 days

Unlimited controllers

Not applicable

More than 55 customers

5-Year

LSS9002300

5 years

1 controller

Once per year

Long-term contracts (up to 5 years)

10-Year

LSS9002400

10 years

1 controller

Once per year

Long-term contracts (up to 10 years)

TIP: Combine one-year subscriptions (1, 5, or 25 controllers) in a single purchase to match your needs and benefit from volume pricing. Example: To access 31 controllers, purchase one pack of 25, one of 5, and one of 1.

Digital Voucher System

Each subscription is delivered as a digital voucher.

Redeeming a voucher:

  • Links the subscription to your Software Shop account.

  • Adds corresponding credits to your digital wallet of your account.

  • Does not activate the subscription immediately.

After redemption, one-year subscriptions for 5 and 25 controllers are automatically converted into a unified format: “1 Controller access fee / Year” for easier management.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.