251020_SpaceLogic_KNX_Remote_SW

eConfigure KNX Users

To use the Remote Configuration Interface with eConfigure KNX, follow these steps to establish a secure remote connection and configure the controller:

Prepare the Controller for Remote Access

Before connecting remotely, ensure the controller is properly configured:

  • Enable Cloud Connectivity
    In the SWITCHBOARD tab, go to Controller > MOBILE APP, and check Enable Cloud connectivity. This prevents disconnection from the cloud after uploading your settings.

Upload Local Parametrization

Once local settings are ready:

  • Go to the UPLOAD tab and select your controller from the list on the left.

  • Click the arrow in the middle of the screen to initiate the upload.

  • In the Potential Security Risk dialog, click Trust to establish the connection.

  • Follow the steps in the upload wizard. The controller will restart to apply IP changes. Ensure your network is aligned with the new controller IP.

  • Click Close to finish.

Connect Remotely via SpaceLogic KNX Remote

  • In SpaceLogic KNX Remote, select the desired controller.

  • Click Connect in the Remote Configuration Interface section.

  • The Configuration IP Address will be displayed.

Configure Access in eConfigure KNX

  • Open the UPLOAD tab in eConfigure KNX and select the controller.

  • Click Select controller access at the bottom left.

  • In the Controller Access dialog:

    • Set Access type to Remote. The controller connects via the Remote Configuration Interface.

  • Click Close.

To verify the connection, go to the UPLOAD tab and click Select interface. The correct interface will appear.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?