251020_SpaceLogic_KNX_Remote_SW

Remote Configuration Interface

The Remote Configuration Interface allows users to remotely access and modify KNX installations using either ETS or eConfigure KNX, as if they were physically onsite. This functionality becomes available once a subscription has been assigned to the controller and the Remote Configuration Interface is enabled.

Once connected, users can perform configuration changes in the ETS (.knxproj) or eConfigure KNX project through a secure VPN tunnel. The interface provides a Configuration IP Address that is used to establish the remote connection.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.