251020_SpaceLogic_KNX_Remote_SW

Filtering Controllers

Filter options: At the top of the screen, you can filter controllers by the following criteria:

  • All

  • Online

  • Offline

  • With Subscription – controllers with a subscription.

  • Without Subscription – controllers without a subscription or with an expired subscription.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?