251020_SpaceLogic_KNX_Remote_SW

SpaceLogic KNX Remote

SpaceLogic KNX Remote is a subscription-based feature designed specifically for system integrators and smart electricians. It works seamlessly with ETS (version 5 or 6) as an ETS App, and with eConfigure KNX (Lite, Expert, and Expert Student, version 3.0 or higher).

With SpaceLogic KNX Remote, you can:

  • Configure KNX installations remotely
    Securely access and configure your customers’ ETS (.knxproj) or eConfigure KNX projects from anywhere.

  • Access and configure controllers remotely
    Gain secure, remote access to your customers’ Wiser for KNX or spaceLYnk controllers for configuration and updates.


Requirements

To use SpaceLogic KNX Remote, make sure you have the following:

Hardware

A Wiser for KNX controller (LSS100100) or a spaceLYnk controller (LSS100200) installed at your customer’s site.

Software

For ETS users

  • ETS 5 or 6

  • SpaceLogic KNX Remote ETS-App

  • SpaceLogic KNX Remote package

For eConfigure KNX users

  • eConfigure KNX Lite, Expert, or Expert Student (version 3.0 or higher)

  • SpaceLogic KNX Remote package

Only 64-bit (x64) versions of Windows are supported for ETS5 and ETS6. Supported operating systems:

  • Microsoft Windows 10 x64

  • Microsoft Windows 11 x64

Subscriptions

To remotely connect to each customer installation – or to your own controller – you will need an active SpaceLogic KNX Remote subscription. Each subscription must be assigned to the specific controller(s) you want to manage.

Preconditions

  • Accessing SpaceLogic KNX Remote is straightforward; use your login credentials for the Wiser KNX mobile app.

  • If you do not use the Wiser KNX mobile app, you will need to register for a new account on Schneider Electric Cloud Services.

  • SpaceLogic KNX Remote is a subscription-based service, which means a valid subscription must be purchased to use it. You will need to register, complete the payment process, and assign the subscription to the controller(s) you wish to manage.
    If needed, you can invoice your customers for reimbursement afterward, or include the subscription cost in the initial project budget. (For details on how to purchase subscriptions, see Purchasing Subscriptions.)

  • To enable remote configuration, the controller owner must provide you with Remote Configuration Access. This permission is essential for connecting to their controller and managing the installation remotely. See more in Remote Configuration Access)

  • If you are not an eConfigure KNX user and you use ETS instead, you can install the SpaceLogic KNX Remote ETS-App into ETS (see more in Installing and Accessing SpaceLogic KNX Remote).

  • SpaceLogic KNX Remote is included in all editions of eConfigure KNX:

    • eConfigure KNX Lite (for ETS 5 or 6)

    • eConfigure KNX Expert (for ETS 5 or 6)

    • eConfigure KNX Expert Student (for ETS 5 or 6)

  • If you are using eConfigure KNX, make sure it is updated to version 3.0 or higher before installing the SpaceLogic KNX Remote package. Refer to the chapter Compatibility and Software Installation of the eConfigure KNX user guide.

  • To enable remote configuration of your KNX installation using SpaceLogic KNX Remote, the Cloud Connector must first be set up and activated on your controller.
    The Cloud Connector can be enabled by the end user if they have access to their controller, or by the system integrator once they have been granted remote access to the controller.
    The Cloud Connector acts as a secure communication bridge between your local installation and the cloud-based remote access services. Without it, remote configuration through ETS or eConfigure KNX is not possible.

  • Management plugin must be installed on the controller as described in Remote Configuration Access.

  • Remote Project Configuration must be enabled via the Management plugin as described in Remote Configuration Access.

Video Tutorial

For additional guidance, watch our official video tutorial:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.