251020_SpaceLogic_KNX_Remote_SW

Releasing Subscriptions

If a controller no longer requires remote access, you can release its assigned subscription for reuse.

Reassignment Limits:

  • 1-Year Subscriptions: Can be reassigned once every 30 days.

  • 5-Year and 10-Year Subscriptions: Can be reassigned once every year.

  • Monthly subscriptions cannot be reassigned to a different controller.

  • The system tracks these timelines automatically – no manual tracking needed.

Steps to Release

  1. Wait for Eligibility

    • After the required period, the Assigned button changes to Release Subscription (dark gray).

  2. Click Release Subscription

    • This returns the subscription to your pool of available subscriptions.

  3. Reassign as Needed

    • You can now assign the released subscription to another controller using the standard assignment process (Assigning Subscriptions).

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.