251020_SpaceLogic_KNX_Remote_SW

Getting Started

ETS Users

After installing the SpaceLogic KNX Remote ETS-App:

  1. Open your KNX project in ETS.

  2. Go to the Apps tab in the ETS menu.

  3. Select SpaceLogic KNX Remote to launch the feature.

This gives you access to remote configuration tools directly within your ETS environment.

eConfigure KNX Users

Once you have upgraded to eConfigure KNX version 3.0 or higher:

  1. Click the hamburger menu (three horizontal lines) in the top-left corner of the screen.

  2. From the menu list, select SpaceLogic KNX Remote.

You will now be able to access all remote configuration features from within eConfigure KNX.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?