251020_SpaceLogic_KNX_Remote_SW

Assigning Subscriptions

To start using the SpaceLogic KNX Remote feature, you must assign your purchased subscriptions to the controllers you want to connect to. This enables secure remote access and full configuration capabilities, including modifying the ETS (.knxproj) or eConfigure KNX project directly within the installation.

Once your subscriptions are created, follow these steps to assign them:

Find the Controller

  • In the controller list, locate the device you want to assign a subscription to.

Assign the Subscription

  • Click Assign Subscription on the controller’s row.

  • In the My Subscriptions dialog, select an available subscription.

  • Click Assign Subscription button to confirm.

Verify Assignment

  • The Assign Subscription button changes to Assigned.

    NOTE: For 1-year subscriptions, after 30 days, the Assigned button will change to Release Subscription for that controller. For 5- and 10-year subscriptions, this change will occur after one year (see more in Releasing Subscriptions).

  • The top-right corner updates to reflect:

    • Remaining available subscriptions

    • Total number of purchased subscriptions

    • By clicking on the information, view details about each subscription you have purchased, including purchase and expiration dates and assignment status.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.