251020_SpaceLogic_KNX_Remote_SW

Cloud Connector Setup

Setting up the Cloud connector ensures that your controller can establish a secure VPN tunnel, allowing authorized users to connect to the system from anywhere, as if they were onsite. This setup is a prerequisite for using the Cloud connector and must be completed before attempting any remote commissioning or updates.

The following steps will guide you through checking, updating, and enabling the Cloud connector on your controller.

  1. Log in to your controller:

    • Open your internet browser and log in to your controller.

  2. Check for latest version:

    • Ensure you have the latest version of the Cloud connector application.

    • To verify, check the list of available applications/updates in the Marketplace.

  3. Update Cloud connector:

    • If you do not have the latest version, click next to the Cloud connector in the application list.

    • It is recommended to check Update automatically to ensure the Cloud connector application is always up-to-date.

  4. Enable Cloud connector:

    • Return to the Start page of your controller.

    • Open the Cloud connector application.

    • Check the box to Enable Cloud connector.

  5. Verify connection:

    • Go back to the Start page and confirm that the Cloud connector is connected.

    • The icon for a correctly connected Cloud connector looks like this:

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.