251020_SpaceLogic_KNX_Remote_SW

Disconnecting the Remote Configuration Interface

You can manually disconnect by clicking the Disconnect button. Otherwise, the interface will automatically disable under the following conditions:

  • ETS or eConfigure KNX is closed.

  • The computer is put to sleep, shut down, or restarted.

  • 24 hours have passed with the software open (for security reasons).

NOTE: If the interface is disabled (manually or automatically), it must be re-enabled as described in ETS Users and eConfigure KNX Users.
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?