251020_SpaceLogic_KNX_Remote_SW

Viewing Controllers

Accessing paired controllers: Once logged in, you will see paired/shared controllers on the Space Logic KNX Remote homepage in ETS or eConfigure KNX Lite.

If your controller does not appear and you have followed all previous steps correctly, click to update the list.

Controller Information

Each controller entry on the homepage displays the following details:

  • Controller name
    Hovering over the name reveals the validity period of access.

  • State
    Indicates whether the controller is online or offline.

  • MAC address
    Unique identifier for the controller.

  • Configuration IP address
    The IP address used for configuration.

  • Edit
    Click to edit controller details.

Control Options

If you have an active SpaceLogic KNX Remote subscription, the following control buttons are available:

  • Assign Subscription / Release Subscription
    Manage subscription assignments.

  • Access
    Remotely access the controller.

  • Connect/Disconnect Connect or disconnect from the configuration interface.

Additional Homepage Buttons

  • Purchase Subscriptions
    Buy new subscriptions for remote access.

  • Help
    Access the full User Guide.

  • Log Out
    Exit the application securely.

Feedback
QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.