251020_SpaceLogic_KNX_Remote_SW

ETS Users

Before using the Remote Configuration Interface in ETS, ensure the controller is commissioned and the ETS project is properly set up.

Steps to connect:

  1. Open your project in the ETS application.

  2. Launch the SpaceLogic KNX Remote ETS-App (see Getting Started).

  3. Locate the controller you want to connect to.

  4. Click Connect in the Remote Configuration Interface section.

  5. Once connected, a Configuration IP Address will be displayed.

  6. Copy the IP address using the copy icon next to the controller.

  7. In ETS:

    • Click to manage connections.

    • Select Manage Configured Connections > Add.

    • Choose IP tunneling.

    • Paste the copied IP address into the Server field and click OK.

You can verify the connection by navigating to the twisted pair icon in ETS, where the corresponding interface will be shown.

QR Code is a registered trademark of DENSO WAVE INCORPORATED in Japan and other countries.

Was this helpful?